The AI Sticky NoteAI 便签屏

The note your family can see.家人都能看到的便签屏。

A dedicated family notes display for reminders, to-dos, warm messages and more.一个家庭专属的便签屏:提醒、待办、暖心留言,一眼可见。

Why Sticky为什么选择 Sticky

Less friction. More visibility. Better follow-through.更少打扰,更多可见,更好跟进。

Sticky is built for the everyday flow of home life - quick add, quick setup and quick glance. Shared visibility for the moments your family shouldn't miss.Sticky 专为家庭日常节奏设计——添加快、设置快、一眼可见。不该错过的时刻,全家一起看见。

Speak to Add开口即记

Press the button and say it out loud. Sticky transcribes your voice into clear notes/to-dos/reminders instantly.按下按键并大声说出来。Sticky 会立即将您的语音转录为清晰的便签、待办或提醒。

Stick Anywhere随处摆放

The magnetic design and accessory let you attach it to any surface — fridge, door, cabinet, you name it.磁吸设计与专属配件让它可以贴在任何表面上——冰箱、房门、柜子,随心所欲。

See at a Glance一瞥即见

E-ink stays on with near-zero power. Your notes are always there when you walk by.电子墨水屏常亮近零功耗,路过时一眼就能看到留言。

Use Cases使用场景

Family notes shouldn't stay buried in a phone.家庭留言,不该被手机埋没。

Features 对比维度
Low Distraction 无电子分心
Quick Update 便捷更新
Hard to Miss 一眼可见
Shared Visibility 共享可见
Setup Simplicity 部署极简
Low Power & Eco-Friendly 低功耗且环保
Sticky Sticky Best Option
Phone App 手机 App
Paper Note 纸质便签
Smart Display 智能大屏

Made for the flow of family routine.为家庭日常而生。

More scenes, less explaining. Show the notes/reminders/info where life actually happens.更多场景,更少解释。把留言、提醒和信息,放在生活真正发生的地方。

Sweet morning notes, right by your bedside.

Sweet morning notes, right by your bedside.清晨的暖心留言,就在床头边。

Tasks assigned right where family life happens the most

Tasks assigned right where family life happens the most家务分派,就在家人常待的地方

To‑dos, clock, weather, notes — a smarter command center, screen by screen.

To‑dos, clock, weather, notes — a smarter command center, screen by screen.待办、时钟、天气、便签——更智能的家庭指挥中心。

One last glance before leaving the door.

One last glance before leaving the door.出门前,再看一眼。

What's inside.内在实力。

Solid hardware with enough openness for developers and makers who want to go further.硬件扎实,也为想深入探索的开发者与创客留足开放空间。

Sticky product features 1 Sticky product features 2
reTerminal sticky reTerminal sticky

Sticky is half-built. You finish it. Sticky 只有一半,由你来完成它。

Facebook Group

Join our growing community加入我们的社区

Early device access开发者先期体验
Vote on next features决定新功能路线
Talk to our engineers与研发工程师对话
Explore & Join the Community 探索并加入社区 .

Newsletter

Join the Waitlist加入候补名单

Subscribe to get early access, launch updates, and exclusive discount when Sticky becomes available. 订阅即可获得抢先体验、上市更新,以及 Sticky 发售时的专属折扣。

Prefer the community? 更喜欢社区? Join the Facebook Group加入 Facebook 群组 or Discord ThreadDiscord 频道

FAQs

Questions, answered.常见问题解答。

What exactly is Sticky?Sticky 究竟是什么?

Sticky is a dedicated magnetic family note device designed for shared visibility at home. Instead of keeping reminders buried in a phone, Sticky makes important notes, to-dos, and warm family messages visible in places like the fridge, kitchen, hallway, or entryway.Sticky 是一款专属的磁吸家庭便签屏,专为家庭成员共同可见而设计。Sticky 不会将提醒埋没在手机里,而是将重要的便签、待办事项和温馨的家庭留言呈现在冰箱、厨房、走廊或玄关等显眼位置。

What makes it different from a smart hub display or an phone app?它与智能中控屏或手机 App 有何不同?

Sticky is intentionally simpler and more focused. A phone is personal and easy to miss. A smart display does many things but is often more distracting. Sticky is built specifically for quick add, quick setup, quick glance moments in shared home spaces.Sticky 更加简单且专注。手机是个人的,容易错过;智能屏功能繁多,但往往更容易让人分心。Sticky 专为共享家庭空间中的“快速添加、快速设置、一眼可见”时刻而打造。

Is the software finalized yet?系统软件目前定型了吗?

We're in active development of the on-device apps and continuously refining the experience based on community feedback. Join our Facebook group or Discord Thread to see the latest updates and influence the product roadmap.我们正处于设备端应用的积极开发阶段,并根据社区反馈持续优化体验。欢迎加入我们的 Facebook 群组Discord 频道 来查看最新动态并共同规划产品路线图。

Can Sticky show the time, weather, or my calendar?Sticky 可以显示时间、天气或日历吗?

Yes! Sticky comes with rich on-device apps including notes, to-do, clock, weather, and image. You can customize what shows on the display through the screen tap or the Seeedash app.是的!Sticky 自带丰富的设备端应用,包括便签、待办、时钟、天气和相册。您可以通过触控屏幕或使用 Seeedash App 来自定义显示内容。

How long does the battery last?电池续航时间有多长?

Thanks to the ultra-low-power E Ink display, Sticky lasts up to one week on a single charge with typical use. For static images or other low‑update‑frequency applications, Battery Saver Mode can extend battery life to several months — though we are still testing the exact runtime.得益于超低功耗的电子墨水屏,在典型使用下,Sticky 单次充电可使用长达一周。对于静态图像或其他低更新频率的应用,省电模式可以将电池寿命延长至数月——不过我们仍在测试确切的运行时间。

Where should I put Sticky in my home?在家里我应该把 Sticky 放在哪里?

With the magnetic design and accessory, Sticky can be attached to any surface. It is ideal for fridges and other household metal surfaces, but it also fits kitchens, entryways, shared family spaces, and any place where visible reminders are most useful.凭借磁吸设计和专属配件,Sticky 可以贴在任何表面上。它非常适合冰箱和其他家用金属表面,但也非常适合厨房、玄关、共享家庭空间以及任何显眼提醒最能发挥作用的地方。

Is Sticky suitable for developers and makers?Sticky 适合开发者和创客吗?

Yes. Sticky is an ESP32-S3 based ePaper display with rich on-board resources and open source development tools and infrastructure for developers to custom build your own on-device apps. We'll release a Doc Center when it's ready so you can later link to technical details, integrations, roadmap updates, APIs, or docs. Stay tuned.是的。Sticky 是一款基于 ESP32-S3 的电子纸显示屏,拥有丰富的板载资源以及开源开发工具和基础设施,供开发人员自定义构建自己的设备端应用。准备就绪后,我们将发布文档中心,以便您稍后链接到技术细节、集成、路线图更新、API 或文档。敬请期待。

What do I get by joining the waitlist?加入候补名单我能获得什么?

Pre-launch product updates, the exact launch date before anyone else, and an exclusive early-bird discount when we go live. Join the email waitlist — just honest updates on how Sticky is coming along.预售产品动态、抢先得知确切的发售日期,以及发售时的专属早鸟折扣。加入我们的 邮件候补名单——只有关于 Sticky 进展的真诚分享。

Where could we download the mobile app?我们在哪里可以下载手机 App?

The Seeedash companion app will be available on both iOS App Store and Google Play Store when we launch. Join our community on Facebook, Discord, or the email waitlist to be notified as soon as it's released.Seeedash 伴侣 App 将在正式发售时上架 iOS App Store 和 Google Play 商店。欢迎加入我们的 Facebook 社区Discord 或订阅 邮件候补名单,以便在发布时第一时间获得通知。

Any doc or tutorial that I can learn how to get started with Sticky?有什么文档或教程可以帮助我快速入门吗?

We're building comprehensive documentation, video tutorials, and a community wiki. Everything from basic quick-start guide to advanced custom on-device app development will be covered.我们正在构建详尽的文档、视频教程和社区 Wiki。内容将涵盖从基础快速入门指南到高级自定义设备端应用开发的所有内容。

Will Sticky support SenseCraft HMI, the no-code ePaper Dashboard design and deployment platform?Sticky 会支持免代码电子纸仪表板设计和部署平台 SenseCraft HMI 吗?

Yes. SenseCraft HMI will eventually be an on‑device app you can opt into through the Seeedash mobile app. For now, there's a dedicated SenseCraft HMI firmware you can flash to Sticky if you want to deploy your HMI designs.是的。SenseCraft HMI 最终将成为一个您可以通过 Seeedash 移动应用选择启用的设备端应用。目前,如果您想部署 HMI 设计,可以为 Sticky 刷入专门的 SenseCraft HMI 固件。