Smart Environmental Monitoring

Meet the Final Batch of 26 Free Hardware Winners! Submit Your Project Documentation to Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022” to Win $18,000+ in Prizes by September 27th

Currently, Seeed Studio is running “IoT Into the Wild Contest for Sustainable Plant 2022” on Hackster.io. To date, we’ve received 207 free hardware applications, along with 500+ people registered as the Contest participants. As the free hardware application has been closed on August 8th, we’ve selected 26 free hardware applicants as the last batch to send out the free hardware kit next week.

IoT Into the Wild Contest for Sustainable Planet 2022: New Judges and Supporters, Last Call for FREE Hardware Application, Special Discounts and Firmware Updates on SenseCAP K1100 Kit!

We’re happy to announce that Semtech, Helium, SOSV, Nova Labs, HAX, Himax, and Chaihuo x.factory have joined Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022” as ‘Judges’ and/or ‘Supporters’. This is your last chance to apply for a free hardware kit by August 8, 2022 – 5 days left! To help assist more participants to use ‘SenseCAP K1100 – The Sensor Prototype Kit with LoRa® and AI’, we’re offering a special discount ($30 off) and free FedEx international shipping option.

Meet the Third Batch of 28 Free Hardware Winners: Submit Your Sustainability Project Ideas to Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022” by August 8th!

Currently, Seeed Studio is running “IoT Into the Wild Contest for Sustainable Plant 2022” on Hackster.io. So far, we’ve received 137 free hardware applications, along with 400+ people registered as the Contest participants. In an effort to inspire a broader number of potential participants, as well as to facilitate the makers and innovators to start their projects early-on, we’ve selected 28 free hardware applicants to send out the free hardware kit next week.

Important Announcement: Helium Award Is Now Added to Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022” & Extended Deadline for Free Hardware Application!

We’re happy to announce that ‘Helium Award’ is now added to Seeed’s open source innovation contest – “IoT Into the Wild Contest for Sustainable Planet 2022”. Funded by Helium, ‘Helium Award’ is designed to select 11 winners in total. With this addition of ‘Helium Award’, we’ve decided to extend the deadline of the free hardware application until August 8, 2022 at 23:59 P.M. (PT).

Meet the Second Batch of 23 Free Hardware Winners: Last Chance to Submit Your Ideas to Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022”!

Currently, Seeed Studio is running “IoT Into the Wild Contest for Sustainable Plant 2022” on Hackster.io. So far, we’ve received 107 free hardware applications, along with 300+ people registered as the Contest participants. In an effort to inspire a broader number of potential participants, as well as to facilitate the makers and innovators to start their projects early-on, we’ve selected 23 free hardware applicants to send out the free hardware kit next week.

Meet the First Batch of 27 Winners to Get a Free Seeed Studio LoRaWAN Dev Kit: Time to Submit Your Ideas to Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022”

Currently, Seeed Studio is running “IoT Into the Wild Contest for Sustainable Plant 2022” on Hackster.io. So far, we’ve received 45 free hardware applications, along with 200+ people registered as the Contest participants. In an effort to inspire a broader number of potential participants, as well as to facilitate the makers and innovators to start their projects early-on, we’ve selected 27 free hardware applicants to send out Seeed Studio LoRaWAN Dev Kit next week.

July 2022: Seeed’s Field Application Engineer Will Be at Dinacon 3 in Sri Lanka for Wild Hacking for a Holistic #IoTIntoTheWild Project Implementation!

To continue the discourse and our efforts on wildlife, biodiversity, and environmental conservation, we’d like to share a good news that Seeed’s Field Application Engineer, Lakshantha Dissanayake, will be joining the 3rd edition of The Digital Naturalism Conference in Batticaloa, Sri Lanka from July 1st to 10th, 2022.

Join Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022” on Hackster to Get 100 Free Hardware and to Win $14,000+ in Prizes!!

Together with Hackster.io, we are very happy to jointly organize “IoT Into the Wild Contest for Sustainable Plant 2022”, which is supported by Project 15 from Microsoft, Zambezi Partners, Edge Impulse, Fab City Foundation, Institute for Advanced Architecture of Catalonia (IAAC), the Paradise International Foundation, Nova Labs, and Helium. We hope that open tech can lay an important foundation for achieving the UN’s Sustainable Development Goals. Through the contest, we hope to encourage more applicable, scalable, plug-and-play, and easy-to-deploy AIoT solutions to solve real-life challenges in the wild.

Earth Day 2022 Special: Calling for Sustainable Fellows for “IoT Into the Wild Initiative” on April 29! Join Us for Wildlife and Environmental Conservation Efforts!

On today’s Earth Day (April 22), Seeed Studio announces an online kick-off meeting for “IoT Into the Wild Initiative” Fellows on 29th of April, to join forces and resources of multi-stakeholders from various sectors for wildlife conservation, climate crisis, carbon neutrality, and environmental conservation efforts.

Follow-Up: Recap of Seeed’s Tech4Good Webinar for the UN ITU’s WSIS Forum 2022

On 18th of March, Seeed Studio hosted a Tech4Good webinar for the UN ITU’s 13th World Summit on the Information Society (WSIS) Forum 2022. Tech4Good webinar has been focused on introducing real-life application cases of AIoT and open source solutions for the most pressing SDG challenges of our time: Carbon Neutrality, Climate Change, Wildlife Conservation, and Sustainable Communities.

Open Source Gears to Conserve the Marine Ecosystem: Hong Kong’s Marine Litter Detective Project Developed by MakerBay, WWF & Seeed

Marine Litter Detective is a GPS-tracking device for monitoring marine pollutants, such as plastics and oil spills. This was developed by WWF Hong Kong in cooperation with MakerBay and Seeed. As a result, this Project has enabled the tracking of the origins and whereabouts of trash floating on the water surface (and inside the marine ecosystem), which disclosed how the marine litter ends up in the ocean from the land. Consequently, the Project can positively influence the UN’s SDGs 14, 6, 3, 17, 13, 11, 12, 4, 9 and 16.

Open Innovation for Marine Pollution: Wind-Powered Sailing Robot “Protei” Is Cleaning Oil Spills, Material Wastes, and Chemical Pollutants in the Ocean

In order to resolve the world’s oil spill issues caused by the Deepwater Horizon Disaster in the Gulf of Mexico, Protei (a wind-powered and automated sailing fleet robot) was developed by MakerBay and Seeed. By shifting its shapes according to water waves and wind directions, the robot has been useful in collecting and cleaning thin sheens of light oil on water surfaces. Thanks to the fact that it is robustly built to survive in harsh weather conditions and hazardous chemical zones, it is now also used to clean material wastes and other chemical pollutants in the ocean. Now, Protei is the ongoing result of glocal open innovation communities. Accordingly, this Project seeks to achieve the UN’s SDGs 6, 14, 11, 15, 3, 1, 7, 9, 8, 12, 13 and 17.

Calendar

January 2025
M T W T F S S
 12345
6789101112
13141516171819
20212223242526
2728293031