SDGs

Follow-Up: Recap of Seeed’s Tech4Good Webinar for the UN ITU’s WSIS Forum 2022

On 18th of March, Seeed Studio hosted a Tech4Good webinar for the UN ITU’s 13th World Summit on the Information Society (WSIS) Forum 2022. Tech4Good webinar has been focused on introducing real-life application cases of AIoT and open source solutions for the most pressing SDG challenges of our time: Carbon Neutrality, Climate Change, Wildlife Conservation, and Sustainable Communities.

Open Source Gears to Conserve the Marine Ecosystem: Hong Kong’s Marine Litter Detective Project Developed by MakerBay, WWF & Seeed

Marine Litter Detective is a GPS-tracking device for monitoring marine pollutants, such as plastics and oil spills. This was developed by WWF Hong Kong in cooperation with MakerBay and Seeed. As a result, this Project has enabled the tracking of the origins and whereabouts of trash floating on the water surface (and inside the marine ecosystem), which disclosed how the marine litter ends up in the ocean from the land. Consequently, the Project can positively influence the UN’s SDGs 14, 6, 3, 17, 13, 11, 12, 4, 9 and 16.

Open Innovation for Marine Pollution: Wind-Powered Sailing Robot “Protei” Is Cleaning Oil Spills, Material Wastes, and Chemical Pollutants in the Ocean

In order to resolve the world’s oil spill issues caused by the Deepwater Horizon Disaster in the Gulf of Mexico, Protei (a wind-powered and automated sailing fleet robot) was developed by MakerBay and Seeed. By shifting its shapes according to water waves and wind directions, the robot has been useful in collecting and cleaning thin sheens of light oil on water surfaces. Thanks to the fact that it is robustly built to survive in harsh weather conditions and hazardous chemical zones, it is now also used to clean material wastes and other chemical pollutants in the ocean. Now, Protei is the ongoing result of glocal open innovation communities. Accordingly, this Project seeks to achieve the UN’s SDGs 6, 14, 11, 15, 3, 1, 7, 9, 8, 12, 13 and 17.

“Smart Citizen Kit” by Fab Lab Barcelona, European Commission and Seeed Going Global: Environmental Monitoring for Civic Participation in Urban and Suburban Communities

Smart Citizen Kit is a completely open-source environmental monitoring device developed for the global Smart Citizen Project by Seeed, Fab Lab Barcelona, IAAC, and European Commision. This Kit allows citizens to easily measure, collect, integrate, and visualize data on an openly-shared platform that will help the citizens to tackle local challenges in their communities. This Project seeks to influence the UN’s SDGs 1, 12, 3, 16, 17, 13, 4, 6, 10, 5 and 9.

#MonthlyWrap-up October: AIoT, LoRaWAN, OpenWrt, AI for Good, Raspberry Pi, ML, Zephyr, and More…

For this entry, we’ll cover 3 breaking news that you might want to know about, 6 awesome projects from the community, 4 stories on how to deploy IIoT Solution to solve real-world issues, 6 technical write-ups, 1 successful manufacturing case, and 2 prototyping news. Hot topics such as SDGs, LoRaWAN, OpenWrt, ML, TinyML, Raspberry Pi, AIoT, Raspberry Pi, and more will be also covered.

Calendar

January 2025
M T W T F S S
 12345
6789101112
13141516171819
20212223242526
2728293031