Open Innovation

Open Source Gears to Conserve the Marine Ecosystem: Hong Kong’s Marine Litter Detective Project Developed by MakerBay, WWF & Seeed

Marine Litter Detective is a GPS-tracking device for monitoring marine pollutants, such as plastics and oil spills. This was developed by WWF Hong Kong in cooperation with MakerBay and Seeed. As a result, this Project has enabled the tracking of the origins and whereabouts of trash floating on the water surface (and inside the marine ecosystem), which disclosed how the marine litter ends up in the ocean from the land. Consequently, the Project can positively influence the UN’s SDGs 14, 6, 3, 17, 13, 11, 12, 4, 9 and 16.

Open Innovation for Marine Pollution: Wind-Powered Sailing Robot “Protei” Is Cleaning Oil Spills, Material Wastes, and Chemical Pollutants in the Ocean

In order to resolve the world’s oil spill issues caused by the Deepwater Horizon Disaster in the Gulf of Mexico, Protei (a wind-powered and automated sailing fleet robot) was developed by MakerBay and Seeed. By shifting its shapes according to water waves and wind directions, the robot has been useful in collecting and cleaning thin sheens of light oil on water surfaces. Thanks to the fact that it is robustly built to survive in harsh weather conditions and hazardous chemical zones, it is now also used to clean material wastes and other chemical pollutants in the ocean. Now, Protei is the ongoing result of glocal open innovation communities. Accordingly, this Project seeks to achieve the UN’s SDGs 6, 14, 11, 15, 3, 1, 7, 9, 8, 12, 13 and 17.

“Smart Citizen Kit” by Fab Lab Barcelona, European Commission and Seeed Going Global: Environmental Monitoring for Civic Participation in Urban and Suburban Communities

Smart Citizen Kit is a completely open-source environmental monitoring device developed for the global Smart Citizen Project by Seeed, Fab Lab Barcelona, IAAC, and European Commision. This Kit allows citizens to easily measure, collect, integrate, and visualize data on an openly-shared platform that will help the citizens to tackle local challenges in their communities. This Project seeks to influence the UN’s SDGs 1, 12, 3, 16, 17, 13, 4, 6, 10, 5 and 9.

Calendar

May 2025
M T W T F S S
 1234
567891011
12131415161718
19202122232425
262728293031