Marine Pollution

Join Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022” on Hackster to Get 100 Free Hardware and to Win $14,000+ in Prizes!!

Together with Hackster.io, we are very happy to jointly organize “IoT Into the Wild Contest for Sustainable Plant 2022”, which is supported by Project 15 from Microsoft, Zambezi Partners, Edge Impulse, Fab City Foundation, Institute for Advanced Architecture of Catalonia (IAAC), the Paradise International Foundation, Nova Labs, and Helium. We hope that open tech can lay an important foundation for achieving the UN’s Sustainable Development Goals. Through the contest, we hope to encourage more applicable, scalable, plug-and-play, and easy-to-deploy AIoT solutions to solve real-life challenges in the wild.

Earth Day 2022 Special: Calling for Sustainable Fellows for “IoT Into the Wild Initiative” on April 29! Join Us for Wildlife and Environmental Conservation Efforts!

On today’s Earth Day (April 22), Seeed Studio announces an online kick-off meeting for “IoT Into the Wild Initiative” Fellows on 29th of April, to join forces and resources of multi-stakeholders from various sectors for wildlife conservation, climate crisis, carbon neutrality, and environmental conservation efforts.

Follow-Up: Recap of Seeed’s Tech4Good Webinar for the UN ITU’s WSIS Forum 2022

On 18th of March, Seeed Studio hosted a Tech4Good webinar for the UN ITU’s 13th World Summit on the Information Society (WSIS) Forum 2022. Tech4Good webinar has been focused on introducing real-life application cases of AIoT and open source solutions for the most pressing SDG challenges of our time: Carbon Neutrality, Climate Change, Wildlife Conservation, and Sustainable Communities.

Open Source Gears to Conserve the Marine Ecosystem: Hong Kong’s Marine Litter Detective Project Developed by MakerBay, WWF & Seeed

Marine Litter Detective is a GPS-tracking device for monitoring marine pollutants, such as plastics and oil spills. This was developed by WWF Hong Kong in cooperation with MakerBay and Seeed. As a result, this Project has enabled the tracking of the origins and whereabouts of trash floating on the water surface (and inside the marine ecosystem), which disclosed how the marine litter ends up in the ocean from the land. Consequently, the Project can positively influence the UN’s SDGs 14, 6, 3, 17, 13, 11, 12, 4, 9 and 16.

Open Innovation for Marine Pollution: Wind-Powered Sailing Robot “Protei” Is Cleaning Oil Spills, Material Wastes, and Chemical Pollutants in the Ocean

In order to resolve the world’s oil spill issues caused by the Deepwater Horizon Disaster in the Gulf of Mexico, Protei (a wind-powered and automated sailing fleet robot) was developed by MakerBay and Seeed. By shifting its shapes according to water waves and wind directions, the robot has been useful in collecting and cleaning thin sheens of light oil on water surfaces. Thanks to the fact that it is robustly built to survive in harsh weather conditions and hazardous chemical zones, it is now also used to clean material wastes and other chemical pollutants in the ocean. Now, Protei is the ongoing result of glocal open innovation communities. Accordingly, this Project seeks to achieve the UN’s SDGs 6, 14, 11, 15, 3, 1, 7, 9, 8, 12, 13 and 17.

Calendar

January 2025
M T W T F S S
 12345
6789101112
13141516171819
20212223242526
2728293031