What is Industrial IoT? [Case Studies]
With the fourth industrial revolution, Industry 4.0, the Internet of Things has become the hot
With the fourth industrial revolution, Industry 4.0, the Internet of Things has become the hot
Seeed IIoT products SenseCAP series are shortlisted for “Green Tech Catalog 2020”, with recognition from the industry for the product quality and its economical and social benefits.
LoRa is a long-range and lower-power wireless communication system providing attractive features that are critical for application in Industrial IoT.
SenseCAP LoRaWAN Light Sensor is aimed for use in outdoor environment with direct exposure to sunlight, and the products need to be waterproof and durable. This post shares how we tested two aspects of the product.
The industrial IoT products must meet the standards of robustness, reliability, and accuracy. Check out how we tested different materials, and chose the optimal enclosure material for LoRa sensor probe.
LoRa products are known for long-range communication, and we’ve put our products into field tests to make sure they meet the standards. Learn how we tested the long-range features of our industrial IoT products – SenseCAP LoRaWAN series.
On Jan 30~31, 2020, Seeed participated in The Things Conference, the World’s largest LoRaWAN Conference organized by The Things Network, in Amsterdam, the Netherlands. Seeed showcased SenseCAP, the industrial IoT LoRaWAN series products, hosted a workshop, gave a keynote speech, and received an interview at the conference.
Is SenseCAP still waterproof after enduring sharp temperature changes? We put the products into 144 hours of testing at extreme temperature (-40 ℃ to 85℃)!
What is IP66? What testing procedures did Seeed SenseCAP LoRaWAN products go through to be rated as IP66?
Located in the North China Plain, the small city of Dingzhou has a strong focus
Yinhai District of Beihai City in Guangxi Zhuang Autonomous Region, with 18,000 hectares of arable