- This event has passed.
Come Visit us at IoT Solutions World Congress 2018 (Barcelona)
October 16, 2018 @ 9:00 am - October 18, 2018 @ 7:00 pm

Setting up our booth!
Date: October 16-18th, 2018
Venue: Booth #A122, Fira Barcelona Gran Via(Hall 2), Barcelona, Spain
Hey Community,
We’re exhibiting at the IoT Solutions World Congress on October 16-18th in Barcelona! We’ve brought 4 solution demos to display this time, including Grove X for IoTea, Azure Sphere, ReButton, and ReSpeaker.
Grove X for IoTea consists of sensors, nodes, and gateways and it collects real-time data of factors that may affect the quality of tea during cultivation and production processes, including temperature and humidity, CO2, O2, PM, and light exposure. The data is collected by the sensors, sent by the nodes to the gateway and eventually to the cloud, and is made accessible to end customers on a webpage. This solution aims to assist tea farmers better manage plantations without altering the traditional practices of tea cultivation and to present real-time environmental data from the plantations on an open platform.
The Azure Sphere demo simulates a fan with IoT connectivity, people can measure the ambient temperature and set up a threshold value to turn on/off the fan from Azure Cloud. MT3620 Dev kit performs as an MCU, which connects with a temperature sensor(SHT31), relay, fan, display, analog device. The temperature value will be on the LED display. Users can swap the resistor to change the fan’s speed level from 0,1,2,3(0 means switch off the fan).
ReButton is a developer device for simple trigger actions, supporting multiple clicks and long press. In addition, you can connect Seeed Grove sensors to add more data points.
As for the ReSpeaker solution, we’ll demonstrate an off-line automatic speech recognition. You can adjust the light with voice control.
If you are nearby and interested in these solutions, just come say hi and talk with us. Any input is welcome! ??