Announcement of Price Increase on ODYSSEY X86J4105
Dear Customers, Please be advised that Seeed Studio will increase prices up to 15%~20% on
Dear Customers, Please be advised that Seeed Studio will increase prices up to 15%~20% on
With the release of new Raspberry Pi CM4 and its IO board, RPi lovers finally
CUDA 11 has a wealth of features – from platform system software to everything you
When deploying computation-intensive projects on the Jetson platform, I always want to know how to
Compared with Jetson Nano, an important feature comes with Jetson Xavier NX is its M.2
When working on Arduino project with Jetson Nano or Jetson Xavier NX, sometimes we need
YOLOv4 was released at the end of April. It soon gained popularity among the machine
OpenCV is pre-installed on Jetson Nano Developer Kit b01. You can run following code in
Recently, I want to use the PWM signal to control the speed of my DC
When trying to convert yolov3 model to onnx, it reported the following error. Then I
I believe many of you have heard about Homelab and been wondering what is it
We have heard from the community that they want to see ODYSSEY – X86J4105864‘s perforamce
Notifications