All Posts

SenseCAP LoRaWAN in Triticale Farming: Precision Agriculture and Sustainable Livelihood Development in Dingzhou, Northern China

Beishao Triticale Field Project elaborates on a deployment scenario of SenseCAP LoRaWAN gateway and sensors for smart agriculture solutions in a triticale field of Dingzhou City in Northern China. This will advance resource-efficiency, environmental traceability, and sustainable technological applications on the field. As a result, this will facilitate self-empowerment of the farmers to manage their triticale fields more precisely by grasping the crop’s conditions and needs with less labor inputs, and later gain higher yields. Overall, this Project contributes to the UN’s SDGs 1, 2, 3, 4, 6, 7, 8, 9, 10, 11, 12 and 17.

Read More »

Smart Greenhouse for Sustainable Agriculture: SenseCAP LoRaWAN Enables Tropical Fruit Cultivation in Northern China

Laiwu Tropical Fruit Cultivation Project portrays a successful case of our SenseCAP LoRaWAN series applied to smart greenhouse farming of tropical fruits in Northern China. Through this Project, Northern farmers are equipped with new knowledge on automated greenhouse control, and the value of precision farming. By doing so, the Project can positively influence the UN’s SDGs 10, 2, 1, 8, 9, 12, 11, 16, 13 and 17.

Read More »

Field-Ready IIoT Solution: Precision Animal Husbandry Enabled by Seeed’s SenseCAP LoRaWAN Hardwares and Machinechat’s JEDI One Software

In order to accelerate precision farming to maintain an optimal level of environmental conditions tailored to the growth and health of livestock in multiple housing sites, Seeed and Machinechat collaborated to make a ready-to-be-deployed IIoT solution, that measures, transfers, aggregates, and visualizes the real-time environmental data of temperature, humidity, light intensity, and air quality.

Read More »

Calendar

2025 年 7 月
 123456
78910111213
14151617181920
21222324252627
28293031