All Posts

Stanford University x Seeed: Open Source Haptic Device for Affordable Haptics Education for All

For Stanford University’s open source haptic device called Hapkit, Seeed designed and made an all-in-one controller board called “Hapkit Board” to reduce the costs on microcontrollers and amplifications that support the Hapkit. This Hapkit Project witnessed a dramatic cost reduction in building educational haptic devices compared to previous models, as well as facilitated convenient learning for learners without mechanical knowledge. In this way, this Project contributes to the UN’s SDGs 4, 5 and 17.

Read More »

SenseCAP LoRaWAN Innovation for SDGs: Sweet Melons Grown at Smart Agriculture Demonstration Park in Beihai, China

Smart Agriculture Demonstration Park Project deployed Seeed’s SenseCAP LoRaWAN gateway and sensors for precision agriculture in a greenhouse of sweet melons, which is located in Beihai City of Southern China. Through the IIoT solution, improved resource efficiency and economic productivity have been observed, through which the Project seeks to achieve the UN’s SDGs 13, 3, 17, 10, 11, 9, 8, 2, 1, 4, 6, 7 and 12.

Read More »

SenseCAP LoRaWAN IIoT Solutions for OPEN Global IoT Education Project for Future Jobs and Resilient Livelihoods

In the OPEN Global IoT Education Project, SenseCAP LoRaWAN IIoT solution has been deployed in order to help solve diverse local challenges for children and local communities towards a sustainable and resilient world. Through their participation, they are self-empowered to learn specific skills to prepare for newly emerging jobs in the future. In this way, the Project aims to achieve the UN’s SDGs 4, 5, 12, 11, 13, 9, 8, 17, 6, 7, 14, 15, 2 and 1.

Read More »

Calendar

May 2025
M T W T F S S
 1234
567891011
12131415161718
19202122232425
262728293031