Meet the First Batch of 27 Winners to Get a Free Seeed Studio LoRaWAN Dev Kit: Time to Submit Your Ideas to Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022”
Currently, Seeed Studio is running “IoT Into the Wild Contest for Sustainable Plant 2022” on Hackster.io. So far, we’ve received 45 free hardware applications, along with 200+ people registered as the Contest participants. In an effort to inspire a broader number of potential participants, as well as to facilitate the makers and innovators to start their projects early-on, we’ve selected 27 free hardware applicants to send out Seeed Studio LoRaWAN Dev Kit next week.


Robot Security Guard Patrols Hong Kong Parking Lot using Seeed Edge AI devices
Security Guards

Voice Needed! Ready for a Wio-E5 & ESP32 Powered WiLoBlIno Device?
#Updated on Jul

Seeed and NVIDIA Announce Collaborations in NVIDIA Inception Program in China
In June, Seeed

July 2022: Seeed’s Field Application Engineer Will Be at Dinacon 3 in Sri Lanka for Wild Hacking for a Holistic #IoTIntoTheWild Project Implementation!
To continue the discourse and our efforts on wildlife, biodiversity, and environmental conservation, we’d like to share a good news that Seeed’s Field Application Engineer, Lakshantha Dissanayake, will be joining the 3rd edition of The Digital Naturalism Conference in Batticaloa, Sri Lanka from July 1st to 10th, 2022.


Top 10 Real-World Machine Learning Projects for Beginners to Try in 2022
Emerging techno

EdgeAI2Wild: Integrate BlueROV-2 with NVIDIA Jetson for An Affordable Under-ice Sensing ROV.
Due to climate