Tire Care device with machine learning based on Seeed Studio XIAO nRF52840 Sense
With Machine Learning it is possible to teach the device what is a “regular” break

Smart Jacket for Caving based on Seeed Studio XIAO ESP32C3 and Seeed Studio Wio Terminal
SAJAC is an innovative smart jacket designed specifically for caving expeditions. This jacket incorporates advanced

Coffee Grinder based on Seeed Studio XIAO ESP32C3
A coffee grinder is great for grinding coffee, but what if you wanted to produce

Salt Water Tracker (SWT) based on Seeed Studio XIAO nRF52840 Sense
Saltwater intrusion is a significant problem for rice paddies in Vietnam, as seawater is increasingly

Ring Mouse based on Seeed Studio XIAO nRF52840
The device is HID mouse controller with 4 buttons. There are: left mouse click, right

Seeed Studio Monthly: March Edition Is Here
Hey community, I’m excited to share that Seeed Monthly is back with a new

Seeed Studio Wins “WSIS Prize 2023 Champion” Certificate for Using AIoT for Environment at UN ITU: Global Recognition of IoT2Wild Contest!
On March 15th, Seeed Studio was awarded “WSIS Prize 2023 Champion” prize certificate at the UN ITU, in Geneva, Switzerland. It’s a UN-level of recognition for the success of IoT2Wild Contest 2022 and the usage of ICTs for environment, which was awarded at ITU’s 14th World Summit on the Information Society (WSIS) Forum 2023.

Add an ARM-M3 Cortex Wifi Module to your projects with ease with the New WizFi360 Grove Module from Seeed Studio and Amal Mathew
Need to add WiFi to your project? Consider the WizFi360 WiFi module now in a

Bothered With Unpredictable Thunderstorms? Grove – Lightning Sensor (AS3935) Is Prepared To Hit Seeed Studio Shelves
The Grove system consists of open-source, plug-and-play hardware for modular electronics project building. By providing