Salt Water Tracker (SWT) based on Seeed Studio XIAO nRF52840 Sense
Saltwater intrusion is a significant problem for rice paddies in Vietnam, as seawater is increasingly

Ring Mouse based on Seeed Studio XIAO nRF52840
The device is HID mouse controller with 4 buttons. There are: left mouse click, right

Seeed Studio Monthly: March Edition Is Here
Hey community, I’m excited to share that Seeed Monthly is back with a new

Seeed Studio Wins “WSIS Prize 2023 Champion” Certificate for Using AIoT for Environment at UN ITU: Global Recognition of IoT2Wild Contest!
On March 15th, Seeed Studio was awarded “WSIS Prize 2023 Champion” prize certificate at the UN ITU, in Geneva, Switzerland. It’s a UN-level of recognition for the success of IoT2Wild Contest 2022 and the usage of ICTs for environment, which was awarded at ITU’s 14th World Summit on the Information Society (WSIS) Forum 2023.

Add an ARM-M3 Cortex Wifi Module to your projects with ease with the New WizFi360 Grove Module from Seeed Studio and Amal Mathew
Need to add WiFi to your project? Consider the WizFi360 WiFi module now in a

Bothered With Unpredictable Thunderstorms? Grove – Lightning Sensor (AS3935) Is Prepared To Hit Seeed Studio Shelves
The Grove system consists of open-source, plug-and-play hardware for modular electronics project building. By providing

Open Recruitment of SDG Open Innovation Camp 2023 for Youth from the Greater Bay
17 Goals to Change the World. The 17 Sustainable Development Goals (SDGs) are an important part

Smart Farming Together with Seeed Studio Edge Controller and reTerminal DM
The greenhouse and poultry farming can use sensors to monitor and control environmental parameters for

Sustainable Data for Business Environment Perception in Smart City
Bauta delivered powerful edge video analysis solutions to provide business organizations and local departments an