Deploying Machine Learning on Microcontrollers: How TinyML Enables Sound, Image, and Motion Classification
Updated on Feb 6th, 2024 TinyML, short for Tiny Machine Learning, refers to the deployment

Hello 0x0F
As Seeed is reaching an impressive milestone, here’s a collection of the memories, and adventures from 15 years of creating Seeed Studio.

IoT Food Spoilage System Built by SenseCAP K1100
The Deviridi project is an Internet of Things (IoT) solution designed to monitor food spoilage.

Liquid Classification with TinyML Built by Wio Terminal and Edge Impulse
The Liquid Classification TinyML project is to classify different liquids based on their spectral responses.

Sensing the Future: Unveiling the Power of Grove Sensors based on Sensirion’s chips for a Sustainable and Healthier World
In today’s fast-paced world, where our lives are intertwined with technology, it is crucial to

Solar Panel Monitoring System Built with XIAO ESP32C3
This project provides an affordable and accessible solution for monitoring solar photovoltaic (PV) systems, which

Low-cost, Plug-and-play, and Customizable Air Quality Monitor System Built on ESPHome (No Soldering Required)
This solution uses Home Assistant to monitor the air quality in a room, easy-to-build, and no

Personal Trainer Anywhere: A TinyML Classification Model to Identify the Correct Execution of Gym Exercises
This project is aimed at creating a device that can act as a personal trainer. This

AI-Assisted Pipeline Diagnostics and Inspection w/ mmWave Sensor
This AI-assisted pipeline diagnostics and inspection system with mmWave technology provides an efficient and cost-effective solution for