All Posts

Seeed Monthly Wrap-up for October & November

Seeed Monthly for October & November highlights 10 groundbreaking news stories, 9 fascinating industrial case studies, 7 product and tech updates, 5 “Co-Create with Seeed” campaigns, 6 Seeed Wikis and 1 inspiring projects.

Read More »

Announcing The Amazon Sidewalk Native LPWAN Asset Tracker Dev Kit

Introducing the LPWAN Asset Tracker Dev Kit for Amazon Sidewalk, powered by Semtech LR1110 and Nordic nRF52840 chips. This open-source kit simplifies indoor and outdoor tracking using GNSS, Wi-Fi, and Bluetooth, ensuring compatibility with Amazon Sidewalk. With features like multiple positioning technologies, environmental sensors, and extensive Grove sensor support, developers can create versatile tracking solutions. The kit aligns with Amazon Sidewalk manufacturing standards, making it ideal for scale-up projects with applications ranging from theft prevention to optimizing asset utilization.

Read More »

IOT202 | Building Compliant, Secure Connected Products with Demo Badge for AWS IoT at AWS re:Invent

Another please-do-not-miss-out workshop at the upcoming AWS re:Invent: the IOT202 Connected Products Workshop, where you’ll delve into hands-on learning with a purpose-built practice kit: Demo Badge for AWS IoT. Led by Andrzej Mizerkiewicz and Thomas Kriechbaumer, this workshop explores various AWS IoT connectivity capabilities, including MQTT, Matter, and Amazon Sidewalk. Gain practical insights into the free-to-connect Amazon Sidewalk network using Bluetooth Low Energy and compare it with MQTT connectivity over Wi-Fi on AWS IoT ExpressLink. You can also explore diverse use cases, such as over-the-air updates, location tracking, sensor data ingestion, digital twins, and shadows.

Read More »

Calendar

May 2025
M T W T F S S
 1234
567891011
12131415161718
19202122232425
262728293031