Huge! Waterproof and dustproof button!
These buttons are from our OEM order, they are mistakenly produced as non-ROHS model thus
Evolution!A new powerful USB to Serial converter
UartSB V2.1 adds USB connectivity to your project easily. It’s pluggable to computer USB port
Time machine!
If you want to remove some solder,here is a tool you should have one-L135A Desoldering pump ,
New products from JYE tech
Multiple Usage Programing Adapter Features: ● Compatible with AVR STK200 programming interface ● Compatible with Altera
Super!Seeeduino Catalyst Pack available now!
This is a deluxe pack for Arduino users; it includes Seeeduino, basic components and prototyping platform, various Input and sensors, visual and
Funnel IO remixed by seeedstudio
Funnel I/O (FIO) is an Arduino compatible board designed by Shigeru Kobayashi, based on
RoHS Compliance for Seeeduino
Since many developers asked about if Seeeduino is RoHS compliant, we replaced all the components
Happy New Year!!
2008 is a very special year for all Chinese people, not just because of the Beijing Olympic Games. On May 12th, a huge disaster came and took thousands of people’s life in Sichuan. Many countries lent their helping hand, just like Michael Jackson songs: We are the one. On the last day of 2008, we would state that we are proud to contribute to open source hardware, participate in the community of generosity and inspirations. Thanks to all the friends who supported Seeed Studio, your supporting made us grown. ^^ 2009 is about to come, we will do our best in supporting open source hardware development. On the occasion of the New Year, Please allow us to congratulate you on the arrival of the New Year and to extend to you all our best wishes for your perfect health, your career greater success and lasting prosperity. -Fan on behalf of Seeed Studio