Seeeduino upgraded to Atmega 328
July 19, 2009
2 Comments
We finally got those chips and produced our new seeeduino board: seeeduino V328. It kept
12V LED strip drives by Rainbowduino
July 14, 2009
10 Comments
Rainbowduino isn’t only used to drive the LED matrix but also can be used to
Seeeduino back instock
July 13, 2009
No Comments
I should post this message through Twitter but seems like it was blocked by GOV.
Seeed studio Anniversary!
July 8, 2009
10 Comments
When time comes to 8th july,2009, the anniversary of seeedstudio has arrived. It is a
Burn the Bootloader for Rainbowduino with UartSB
July 3, 2009
1 Comment
The Rainbowduino have not the USB connector and cannot use the Arduino IDE to program
Seeeduino MEGA
June 29, 2009
3 Comments
The Seeeduino Mega is as small as the seeeduino which is about 2/3 of the
Real Time Clock module
June 28, 2009
No Comments
The RTC module is a conventional module in many circuits. You can used it to
Use the Seeeduino as a UartSB
June 22, 2009
1 Comment
As the Rainbowduino sell like hot cakes, more and more Email comes to ask how