Arduino Communication Peripherals: UART, I2C and SPI
UART, I2C and SPI are one of the most common and basic hardware communication peripherals

Arduino GPS Modules – Which one to use? Comparison, Arduino Tutorial, and projects [2025]
Introduction to GPS and GPS Modules You’re probably familiar with GPS as the ones that

Statement on the Naming of Seeeduino Femto
We released the newest addition to our Seeeduino family, the Seeeduino Femto yesterday. Unfortunately, due

Arduino Wifi Modules: Which one to use?
Introduction to Wifi Modules When it comes to WiFi Modules, everyone should have heard about

Arduino Kit – What is inside and What can you do with it?
Interested in coding, electronics and Arduino? Well, an Arduino starter kit will be one of

Arduino Ultrasonic Sensor Overview and Tutorials
With Arduino ultrasonic sensors like the HC-SR04, you can measure the distance. Through this Arduino

Ubuntu 19.10 official support for Raspberry Pi 4 does not support 4GB version
With the release of Ubunutu 19.10, many Raspberry Pi users are excited as Canonical has

Arduino Tutorial: How to drive a DC and Servo Motor
The Arduino has always been used to control motors. A few examples would be the

SCD30: Carbon Dioxide, Humidity, and Temperature all in one
You may be wondering why do the SCD30 looks different from its original product. The