Raspberry Pi 4 Firmware Update – Pi 4 Now Runs Cooler Than Ever
When the Raspberry Pi 4 first launched, everyone was excited about its ground-breaking processing and

Getting started with micro:bit: MakeCode, Accessories, Projects!
What is micro:bit? Introduction The BBC micro:bit is a pocketable computer, ideal for kids and

Getting Started with Arduino Motors – DC, Stepper, Servo Motor
When using the Arduino, there are many projects and things that you can do with

LTE Cat 1 Raspberry Pi Hat: Build faster IoT applications
Need a Cellular Raspberry Pi Hat that allows for faster building of IoT applications? The

Introduction to CAN-BUS and How to use it with Arduino[2025]
Updated on the 03/01/2024 Ever heard of CAN-BUS but don’t exactly know what it does?

Arduino Accelerometers: ADXL356, ADXL345 vs ADXL335
Mems accelerometers are simple, portable, and applicable but how do we get started? Which accelerometer

10 Things you can do with your HX711 and Load Cell
Ever heard of the HX711 and Load Cell? They are commonly used together to create

MLX90640 IR Array: Thermal Imaging Cameras for your Microcontroller
The MLX90640 32×24 IR array by Melexis is a cost-effective alternative unlike the one seen

What is HMI? – Introduction to Human Machine Interface with Nextion
HMI also known as Human Machine Interface, is a display that allows the user to