Arduino Boards Selection Guide
Arduino is an open-source platform that includes both hardware and software. The hardware of Arduino

How to Use Raspberry Pi GPIO Pins – Python Tutorial
Whether it’s the Raspberry Pi 3, 4 or the tiny Raspberry Pi Zero, GPIO pins

Raspbian Big Update release – Tons of new Features
Recently, the Raspberry Pi foundation released a new update for Raspbian, a free operating system

ARM releases Cortex-M55 Core and Ethos-U55 microNPU
Recently, ARM announces its newest addition to its Cortex-M series, the new Cortex M55 Core.

ACS712 Current Sensor: Features, How it works, Arduino Guide
Have you ever stopped and wonder the amount of current each of your electrical appliances

How to Safely Overclock your Raspberry Pi 4 to 2.147GHz
The Raspberry Pi 4 is arguably the best Single Board Computer, but did you know

Types of Resistor and How to Color Decode them
If you’re building an electrical circuit (series or parallel), chances are you’ll require a component

How to use Arduino OLED I2C Display with SSD1306 / SSD1315
The SSD1306 is a popular choice when it comes to picking an OLED 128×64 I2C

New Linux 5.5 – Supports Raspberry Pi 4!
Linux 5.5 which is the latest stable version of the Linux Kernel, features some really