Resource Roundup for ODYSSEY – X86J4125: A Windows 10 Mini PC also Supports Linux OS
We will keep updating more resources and work we have done on this roundup blog. Please stay tuned and feel free to let us know what tests, tutorials, and add-ons you want to see for ODYSSEY – X86J4105!

Wio Terminal Update: How to Integrate with Raspberry Pi and Display the System Data on LCD Screen
Supporting dual-display at resolutions up to 4K, Raspberry Pi is capable of driving almost any

Wio Terminal Update: Build An Affordable IR Thermal Imaging Camera
Now you can make an affordable thermal camera with Wio Terminal and Grove – Infrared

Linux 5.6 Release – New features!
Previously as Linux 5.5 was released, we saw many interesting hardware improvements and features from

Use Seeeduino Xiao to make a Pocket Distance Alarm – making sure others stay one meter away
A portable distance alarm that will give light and sound warning when people get into

Introduction to MicroPython – Python for Microcontrollers
Wish to start programming your microcontrollers and start on your own home automation project? Perhaps
A new i.MX 8M SBC product idea…
The i.MX 8M is an industry-leading application processor that based on Arm® Cortex®-A53 and Cortex-M4 cores

Two PCIe-to-USB bridge chip solution to use NVMe SSD on your Raspberry Pi 4
As we all know that one of the important improvements in Raspberry Pi 4 is
Best Electronics Kits for Kids, Beginners & STEM Education Based on Micro:bit, Grove Zero, and Arduino #Learn from Home
Apply the coupon code [LFH2020] to enjoy 15% OFF for Arduino nano, Arduino Uno, and