Deep Learning Sumo Robot
Hajimete! Let DL pushing madness begin! Original article by Dmitry Maslov published on Hackster.io Robot-sumo, or

User Review: Hacking the M.A.R.K Robot by Philip Mallon
Over the past six weeks I have had the privilege to test an early release

High-Low Temperature Testing of SenseCAP Industrial IoT Products
Is SenseCAP still waterproof after enduring sharp temperature changes? We put the products into 144 hours of testing at extreme temperature (-40 ℃ to 85℃)!

All You Want to Know about ODYSSEY – X86J4105: Don’t Miss Out on Our Q&A!
We have received more and more questions and suggestions for ODYSSEY – X86J4105. Thank you

Updates for Wio Terminal’s Network Connectivity: What does “Wio” Stand For, A Brief Introduction of Realtek RTL8720DN, and How to Connect Wio Terminal to Wi-Fi and Obtain Data from the Internet
Today’s update for Wio Terminal is about one of its highlight features – its reliable

Use Seeeduino XIAO in Kicad PCB Design Like a Components
The half-hole design of Seeeduino XIAO is for soldering directly on the PCB, no connectors
Types of Capacitors and Its Uses
Within the field of consumer electronics, there are various types of components used in electronic

Wio Terminal Update: The Latest Status of Manufacturing, New Factory Firmware to Speed Up the Testing Process, Built-in Magnet and Mounting Hole for Easy Project Setup
During this challenging period, our team has worked hard to optimize the schedule and accelerate
Seeed in the News
Some of Seeed’s coverage in the media, continuously updated. Seeed as a Company eeNews Embedded: