Linux 5.7 Released: New features and Main Changes
The new Linux 5.7 was released recently after being officially announced in an email by

What is a Doppler Radar Sensor and How does It Work?
Introduction When you hear the word Doppler Radar, you might be familiar with the word

The Biggest Ever Open Parts Library! Over 150,000 parts for Seeed Fusion PCBA
The long-awaited expansion is finally here! Yes, now over 150,000 local parts are available in

28 Raspberry Pi Linux Commands: A Quick Guide to Use the Command Line for Raspberry Pi
Introduction When you get your hands on a Raspberry Pi for the very first time,

What’s the difference between MLX90640 and MLX90641 thermal camera?
What’s a thermal camera? A thermal camera is also called an infrared camera or a

Run Different Firewall OS on ODYSSEY X86J4105: pfSense, OPNsense, IPFire, ClearOS, and Endian Firewall.
The firewall is important to network security systems, which help to isolate the network from
The Basics of Filters and the Different Types of Filters
In the field of electronics, filters can be found in almost all electronic devices from

Top 5 Featured Seeeduino/Arduino Grove Projects of the Week – June 11
Welcome back to our Top 5 featured projects section. Here are the Top 5 featured

Thermal Imaging And It’s Applications
Background With the development of new technologies, thermal imaging has come a long way. Thermal