Meet reServer, a Powerful Edge Computing System Closer to the Real World
From the centralized cloud to the decentralized edge.

Seeed joins CAPIAC
Seeed joins CAPIAC for future collaborations in the field of environmental monitoring for smart agriculture.

Learn TinyML using Wio Terminal and Arduino IDE #5 Anomaly detection for Predictive maintenance with new Blynk IoT Platform release
And the topic of this article is Anomalies. Or specifically anomaly detection for predictive maintenance.

9 Ways to Use Industrial IoT for Industrial Safety
The Internet of Things, or IoT in short, is a very important trend of the

Introducing DHT20 Temperature and Humidity Sensor and Comparing it with DHT11!
(Update) Grove – Temperature & Humidity Sensor DHT20 V2.0 Released! Following the release of the

Brand new Raspberry Pi PoE+ HAT is now available at Seeed!
The Raspberry Pi Foundation has just announced the brand new Raspberry Pi PoE+ HAT for

More Wio Terminal Sensors are now Azure IoT Plug & Play Certified!
Ever since the Wio Terminal was Azure IoT Plug & Play Certified in 2020, we’ve

Introducing Seeed’s Wio RP2040 Family – Mini Dev Board & Module!
Seeed is proud to share our brand new Wio RP2040 Family, based on the RP2040

Adding Ethernet to Raspberry Pi Pico – It’s easier than you think!
Released in late January of 2021, Raspberry Pi Pico is a flexible microcontroller board based