Arduino Days Colombia 2025: Empowering Social Impact with Open Hardware and AI
By Gabriel Giraldo 1 week ago
On March 21st and 22nd, nearly 100 participants came together in Manizales, Colombia for Arduino Days Colombia 2025, a celebration of Arduino‘s 20th anniversary. Organized by Gabotrix, the University of Caldas, the University of Manizales, the Manizales Hub of Young AI Leaders (a UN AI for Good initiative), Seeed Studio, and Arduino, the event showcased how open hardware and AI can solve real-world problems aligned with the UN Sustainable Development Goals (SDGs).
Workshop 1: Control Hardware with Generative AI and NLP









In the first hands-on session, participants explored how to control physical devices using AI-generated code and natural language commands. Leveraging tools for generative AI and microcontrollers like the XIAO ESP32S3, they successfully activated buzzers, LEDs, and motors based on user input through voice or text.
At first, many participants were uncertain, wondering how generative AI could simplify controlling hardware. But by the end of the workshop, everyone was surprised by how easily they could activate buzzers, LEDs, and motors based on voice or text input. The simplicity and effectiveness of applying generative AI in such a practical context left everyone feeling accomplished.
Workshop 2: Voice & Vision AI on the Edge with XIAO ESP32S3 Sense + Edge Impulse









The second workshop dove into Voice and Vision AI at the Edge, combining the XIAO ESP32S3 Sense with Edge Impulse. Participants trained and deployed on-device machine learning models capable of object recognition and voice command classification—without relying on cloud services. This approach enabled real-time responses with low latency, ideal for smart sensing applications in remote or resource-constrained environments.
Hackathon: Solving Real-World Problems in Colombia with Open Hardware



















The core of the event was a Hackathon focused on solving local challenges using Arduino, Seeed Studio sensors, and open tech, inspired by ten real problems in Colombia—each tied to one of the SDGs.
The solutions were not only creative but impactful:
DeterFuga: A smart water leak detection system designed for rural areas, using a combination of sensors, real-time alerts, and intelligent processing. This project exemplified how even newcomers to hardware could contribute to tackling critical issues like water loss in rural systems. Check out the project: DeterFuga on Hackster.io
Plataforma Colaborativa de Datos Ambientales: A collaborative platform that collects environmental data (such as air quality, noise, and UV levels), processes it with machine learning, and displays it on an accessible dashboard. This solution highlighted how IoT and machine learning can be used to monitor and visualize environmental conditions in real time. Learn more: Environmental Data Platform on Hackster.io
Participants formed multidisciplinary teams and developed working prototypes in just 20 hours. Each challenge included real data sources, making the problems tangible and the solutions impactful:
Challenge 1 – Smart Agriculture (SDG 2)
Problem: Over 36% of rural communities face poverty and joblessness. Inefficient irrigation impacts food security.
Data: 48% of Colombia’s rural population faces energy and food insecurity. (El País, 2025)
Challenge 2 – Air Quality Monitoring (SDG 3)
Problem: Cities like Bogotá and Medellín face critical air pollution.
Data: PM10 levels exceed 50 µg/m³. (IDEAM/JICA)
Challenge 3 – STEM Education Kit (SDG 4)
Problem: 27% of rural children don’t complete secondary education.
Data: Major educational gaps exist in rural areas. (Javeriana University, 2022)
Challenge 4 – Water Leak Detection (SDG 6)
Problem: Some regions lose 30% of water due to leaks.
Data: Up to 0.5 m³/hr is lost in aging systems. (DNP, 2023)
Challenge 5 – Solar Monitoring Systems (SDG 7)
Problem: Ineffective monitoring reduces the impact of solar energy.
Data: Only 12% of electricity comes from non-conventional renewables. (MinEnergy, 2023)
Challenge 6 – IoT Waste Management (SDG 11)
Problem: Urban recycling rates are below 20%.
Data: Bogotá only recycles 18% of its waste. (District Environment Secretariat)
Challenge 7 – Responsible Consumption Monitoring (SDG 12)
Problem: High levels of energy and water waste.
Data: 30% of urban water is wasted. (DANE, 2023)
Challenge 8 – Low-Cost Weather Station (SDG 13)
Problem: Rural areas lack local climate data.
Data: Fewer than 10% of communities have proper weather stations. (IDEAM)
Challenge 9 – Early Warning System (SDG 13)
Problem: Natural disasters cause major losses.
Data: Colombia loses $3.6 billion annually to climate events. (DNP, 2023)
Challenge 10 – Environmental Data Platform (SDG 17)
Problem: Poor data integration limits environmental response.
Data: Over 40% of cities lack integrated systems. (DNP, 2022)

During the event, we proudly announced the global launch of the Interactive Signage Contest 2025! From voice-activated doorplates to classroom boards that update in real time, this contest invites makers to design open-source signage powered by AI, IoT, and Seeed Studio hardware.
Selected projects will receive:
Prototyping support
Co-Create collaboration
Seed funding
A fast track to present at Maker Faire Shenzhen 2025
Partners include: Chaihuo Maker Space, Hackster.io, Make:, ICTP, Fab Foundation, Supplyframe, MakerGram, Gabotrix and others.
More Information: https://www.seeedstudio.com/blog/join-seeeds-interactive-signage-contest-2025/
Thank You, Colombia
As a Seeed Ranger, it was fulfilling to see how the collaboration between the different partners made this event a success. From guiding participants through the workshops to helping them with the challenges in the hackathon, my role was not only about providing technical assistance but also about empowering everyone to see how open hardware and AI can be transformative.
Arduino Days Colombia 2025 wasn’t just a celebration—it was a movement. Thank you to everyone who helped spark innovation that truly matters.
Let’s keep building. Let’s keep solving.
Powered by Seeed Studio – your global partner in AI + IoT prototyping.