Let’s Type Cooler with KeebSupply Keyboards: Zilpzalp and GEIST TOTEM, Powered by Seeed Studio XIAO
At KeebSupply, a passion for unique, high-quality mechanical keyboards has transformed a small hobby into a thriving business for Jakob, Conor, and Timur. Initially, Jakob and Conor’s tinkering led them to design a modest macropad in 2020, sparking a love for designing custom keyboards that’s only grown. Today, the KeebSupply team brings users thoughtful, meticulously crafted designs that balance simplicity with innovation, inviting keyboard enthusiasts of all skill levels to create and customize their perfect setup.

With each product, KeebSupply aims to empower hobbyists and designers alike by creating versatile, customizable keyboards built around open-source principles. Collaborating with artists and designers in the mechanical keyboard community, the team develops products that support the DIY ethos, using quality materials and components while prioritizing accessibility.
Today, let’s dive into two of their very special innovations, Zilpzalp and GEIST TOTEM, to see how KeebSupply combines simplicity, community-driven design, and advanced tech with the tiny but powerful Seeed Studio XIAO controllers.
The Zilpzalp Keyboard: Compact, Portable, and Minimalist, Powered by XIAO RP2040
Source: KeebSupply
The Zilpzalp, designed by kilipan, brings a unique take to the unibody-split keyboard format. With just 28 keys, the Zilpzalp is a column-staggered keyboard that maintains the precision and functionality of a full-sized keyboard in a much smaller footprint. Its minimalist layout makes it a great choice for anyone prioritizing compactness without compromising on ergonomic features.
Central to the Zilpzalp’s design is the Seeed Studio XIAO RP2040 microcontroller, a compact yet powerful component that supports both QMK and ZMK firmware for wired and wireless configurations, respectively. The Zilpzalp offers various switch versions, including Choc and MX, with options for both hot-swap sockets and solder-only setups, so users can fully customize their tactile experience. Thanks to FOSS tools like KiCad and Ergogen, the keyboard’s PCB layout is open-source, inviting more customization options.

The Zilpzalp is ideal for minimalist enthusiasts who want a small, portable keyboard without sacrificing style or performance. Its compact nature makes it perfect for travelers, desk minimalists, and anyone looking to explore compact keyboards for the first time.
The GEIST TOTEM Keyboard: A Versatile, Ergonomic Split Design, Powered by XIAO nRF52840 and XIAO RP2040
Source: KeebSupply
GEIST TOTEM, a collaborative project between KeebSupply and designer GEIST, is a 38-key, column-staggered split keyboard designed with both comfort and flexibility in mind. TOTEM is a great fit for those who prefer a low-profile, ergonomic setup, as it comes with a split layout to help reduce strain on the fingers and wrists during long sessions.
The TOTEM kit comes in a wired and wireless variant. The wired version runs on the XIAO RP2040, while the wireless model uses the XIAO nRF52840 for seamless Bluetooth connectivity. Designed with beginners in mind, TOTEM includes pre-soldered diodes to streamline the assembly process. Each kit comes standard with a durable SLA 3D-printed black resin case, ensuring a sleek and sturdy build. For those seeking maximum convenience, a fully assembled kit option is also available, making it easy to dive into the world of custom keyboards.
Source: KeebSupply
It’s noteworthy that GEIST TOTEM won the first prize award in the Seeed Fusion DIY XIAO Mechanical Keyboard Contest back in 2022. It’s always exciting to see projects like this flourish in the community, thanks to KeebSupply.
The KeebSupply Experience
Whether you’re a DIY keyboard enthusiast or a newcomer to custom keyboards, KeebSupply’s Zilpzalp and TOTEM models bring something truly special to the table. These keyboards showcase the team’s commitment to accessible, high-quality designs, allowing users to personalize their typing experience fully. KeebSupply’s collaboration with designers like GEIST and kilipan reflects their passion for open-source designs and their support for the keyboard community.
For more about Zilpzalp, TOTEM, or any of KeebSupply’s projects, head over to their website.
End Note
Hey community, we’re curating a monthly newsletter centering around the beloved Seeed Studio XIAO. If you want to stay up-to-date with:
️ Cool Projects from the Community to get inspiration and tutorials
Product Updates: firmware update, new product spoiler
Wiki Updates: new wikis + wiki contribution
News: events, contests, and other community stuff
Please click the image below to subscribe now!