ReSpeaker Lite Updates: New Firmware, Enclosure Tips and Installation Guide!
The ReSpeaker Lite Voice Assistant Kit has been available to community for some time, and thanks to your feedback, we’re thrilled to introduce several exciting updates! These enhancements make it even easier for voice assistant enthusiasts and DIYers to build their projects.

We recommend purchasing products from the ReSpeaker Lite Voice Assistant Kit, which includes:
2) ReSpeaker Lite with XIAO ESP32S3
3)Mono Enclosed Speaker – 4R 5W
4)Acrylic Enclosure for ReSpeaker Lite
You can mix and match as you like.、
Firmware Update for Better Performance
We’ve updated the firmware to boost performance across the board. Be sure to download the latest version that matches your setup:
- USB version (for the ReSpeaker Lite):
respeaker_lite_usb_xmos_v2.0.5.bin
- I2S version (for the ReSpeaker Lite with XIAO ESP32S3):
respeaker_lite_i2s_xiao_1.0.7.bin
Check out our Firmware Upgrade Guide for step-by-step instructions.
Enclosure Installation Instruction
We’ve also added a detailed, easy-to-follow enclosure installation guide to help you safely assemble your ReSpeaker Lite setup. Watch the video and ensure your device is perfectly housed and ready to use:
Custom Enclosure Design Recommendations
If you’re designing your own enclosure, here are some important guidelines to ensure optimal audio performance:
- Ensure that the distance between the speaker and the two microphones is uniform, and minimize the transmission of speaker vibrations to the microphones to maintain audio clarity.
- The enclosure should allow human voice to reach each microphone without obstruction, ensuring direct sound (as opposed to reflected sound) can evenly reach both microphones for accurate sound capture.
- If you are designing a sealed microphone chamber, avoid creating a resonant cavity that is narrow at both ends and wide in the middle, as this can interfere with front-end signal processing. If a sealed chamber is not feasible, incorporate multiple perforations in the enclosure to prevent sound reflections from bouncing inside before reaching the microphones. This helps to maintain signal integrity.
Beginner Tips for Easier Soldering
For beginners, we recommend using pin headers when soldering components. This makes the process smoother and helps reduce errors—perfect for those just getting started.
Get Involved and Stay Updated
We’re continuously working on more improvements, so stay tuned for future updates! In the meantime, check out our wiki for in-depth technical details. Have questions, suggestions, or ideas for new features or products? Drop them in the comments below—we’d love to hear from you!
For hardware customization, bulk orders, or distribution inquiries, please contact us at iot@seeed.cc.