Meet Seeed Studio XIAO RP2350, the Smallest MicroPython-Ready Dev Board Powered by Raspberry Pi RP2350

The new XIAO RP2350 packs the capabilities of the Raspberry Pi RP2350 chip into the beloved XIAO form factor. And it still manages to include 19 GPIOs, an RGB LED, battery management, and more.

It’s yet another exciting release from Raspberry Pi today (for the Raspberry Pi Pico 2 and RP2350 chipset)! And here at Seeed we’re excited to announce Seeed Studio’s latest release – the XIAO RP2350! This tiny board packs the capabilities of the Raspberry Pi RP2350 chip into the beloved XIAO form factor, making it one of the smallest dev board for MicroPython. XIAO RP2350 is already featured in the Powered by Raspberry Pi Product Catalogue among with other solutions based on RP2350.

As one of the smallest MicroPython-ready dev boards available, the XIAO RP2350 is perfect for space-constrained projects that require high performance. It has all the features of the RP2350, including dual-core, dual-architecture capability, allowing developers to switch between the dual industry-standard Arm Cortex-M33 cores @ 150MHz with FPU, and dual Hazard3 RISC‑V cores, security features like secure boot and an encrypted bootloader. Despite its small 21×17.8mm size, it still manages to include 19 GPIOs, an RGB LED, battery management, and more.

1 XIAO RP2350 = 2 Gummy Bears

Best of all, the XIAO RP2350 is compatible with tons of add-ons through the XIAO ecosystem. You can easily add displays, sensors, motors, LED matrix, expansion boards and more. It supports MicroPython, C and C++ right out of the box too.

Some highlighted features:

  • 19 GPIOs (8 more than previous XIAOs!) allowing more complex projects
  • Powerful dual-core and dual-architecture (Arm and RISC-V) RP2350 chip with FPU for demanding applications
  • Security features like secure boot and encrypted bootloader protect your code
  • Runs MicroPython, C and C++ for maximum flexibility
  • Extensive ecosystem of add-ons like Grove sensors, actuators, displays, LED matrix and more

The XIAO RP2350 is in stock now with a limited first batch of 400 boards on both our Webstore and AliExpress Store. Don’t miss your chance to be one of the first to try out this tiny powerhouse – check out our product page today. Let me know if you have any other questions!

Join Our Early Adopter Program

To assist developers in adapting their projects to the XIAO RP2350 quickly, we’re launching an early adopter program. If you’re an author or maintainer of a popular open-source Raspberry Pi project on GitHub, or an influencer on platforms like YouTube or Tiktok or Instagram, make sure your users can run your code on the XIAO RP2350. Join to receive 2 free boards and technical support to make your code compatible with this exciting new board.

Notes at the end.

Hey community, we’re curating a monthly newsletter centering around the beloved Seeed Studio XIAO. If you want to stay up-to-date with:

🤖️ Cool Projects from the Community to get inspiration and tutorials
📰 Product Updates: firmware update, new product spoiler
📖 Wiki Updates: new wikis + wiki contribution
📣 News: events, contests, and other community stuff

Please click the image below👇 to subscribe now!

About Author

3 thoughts on “Meet Seeed Studio XIAO RP2350, the Smallest MicroPython-Ready Dev Board Powered by Raspberry Pi RP2350”

Comments are closed.

Calendar

August 2024
M T W T F S S
 1234
567891011
12131415161718
19202122232425
262728293031