Introducing the World’s First IP65-Rated Meshtastic Tracker Device, SenseCAP T1000-E
Imagine you’re in a place with no 4G, 5G, or WiFi. How would you stay
Imagine you’re in a place with no 4G, 5G, or WiFi. How would you stay
Updated: Mar 5, 2025 In the world of smart homes, selecting the right hardware is
The “Bathing Water Quality” project at Boscombe Seafront, Bournemouth, marks a significant advancement in coastal
FAB24 Mexico, hosted by The Fab Foundation, Fab City Foundation, The Center for Bits and
Ever wished your Tesla could make a statement even when you’re slowing down? Seth Evans,
Hey community, we’re pleased to announce that Seeed Studio has partnered with KaaIoT to provide
Introduction Back in 2019, the concept of the “MING” stack—comprising MQTT, InfluxDB, Node-RED, and Grafana—was
Along the last decade I’ve had the possibility to host Lutòpia, a wearable & decorations
The XIAO RA4M1 maintains the beloved features of the Seeed Studio family: a thumb-sized form factor, all components surface-mounted with stamp holes on both sides, compatibility with Seeed Studio XIAO accessories, and open-source availability. It also boasts the Renesas’ RA4M1 32-bit ARM® Cortex®-M4 running at up to 48 MHz with FPU, along with ample memory and flash storage.
Image source: AI-generated In modern computing, the CPU (Central Processing Unit), GPU (Graphics Processing Unit),
Boost your knowledge with 12 in-depth tech exploration offering expert insight, 4 fascinating livestream recap, 10 product and service showcases that will leave you in awe. Plus, prepare for 7 latest Seeed news and event highlights. Dive into the vibrant open-source community with 4 inspiring projects.
Have you ever wanted to access real-time coverage of public LoRaWAN® networks and find the
Notifications