We’re excited to announce that Seeed Studio will be exhibiting at embedded world 2024, one of the premier events in the embedded systems industry. The trade show will take place from April 9th to 11th, 2024 at the Nuremberg Exhibition Centre. At Booth 4-551, Seeed Studio will proudly present a diverse range of Open Source AI Hardware products, designed to empower developers and innovators in their projects.
Besides the rich lineup of products and demos at the Seeed booth, we’re excited to share that our valued partners will also feature a wide range of exhibits with Seeed products and services.
Get ready to discover a world of innovative products, exciting demos, and practical solutions at our valued partners’ booths. Here is a sneak peek! We encourage you to visit their booths and engage with the demos firsthand to explore potential opportunities for collaboration.
1.AWS: Booth 4-552
At AWS’s booth (4-552), you will be able to see AWS’s vision of Gen AI & IoT Chess Robot, powered by AWS Bedrock and Seeed’s Jetson devices.
We also have a kiosk at AWS’ Booth centering around our joint demo of Dual-Network Tracking Solutions with Amazon Sidewalk and LoRaWAN.Traditional asset tracking can suffer from network coverage limitations. Dual-network tracking solutions with Amazon Sidewalk and LoRaWAN address this challenge. Experience seamless LPWAN network roaming with this asset-tracking demo. Featuring the Seeed Studio Wio Tracker Dev Board and robust SenseCAP T1000-S Tracker device, both powered by Semtech LR1110 and Nodic Semiconducter’s nRF52840, the setup demonstrates seamless transitions between LoRaWAN and Amazon Sidewalk networks unified by AWS IoT Core. Experience the future of low-power wide-area connectivity with this solution’s versatility for real-time asset tracking and utility metering applications.
![](https://www.seeedstudio.com/blog/wp-content/uploads/2024/04/image-773x1030.jpg)
AWS also organizes an IoT Demo Badge Workshop. Attendees of this workshop will gain practical experience in securely connecting IoT products and managing them through AWS IoT services. With the help of a specialized educational device known as the Demo Badge, participants can discover various AWS IoT connectivity options.The Demo badge is also one of the Co-Create products from Seeed Studio Fusion.
Date: Wednesday April 10, 2024
Start Time: 2:00 PM local Germany time
Where: Nuremberg Messe, NCC Mitte, Munchen 2
![](https://www.seeedstudio.com/blog/wp-content/uploads/2024/04/AWS-workshop-image-1030x483.png)
2.PNY: Booth 3-539
Seeed Studio is glad to partner with PNY Technologies, Inc., a global supplier of components and NVIDIA solutions for the artificial intelligence, HPC, data center, and professional visualization markets. The partnership represents a convergence of Seeed Studio’s expertise in AIoT hardware, particularly as an Elite Partner in the NVIDIA Jetson ecosystem, with PNY’s comprehensive edge AI platforms tailored for Smart Cities & Spaces. The collaboration is designed to enhance the accessibility, efficiency, and streamlined deployment of advanced AI technologies for developers and businesses worldwide. At the upcoming Embedded World 2024 in Nuremberg, they will showcase highlighted NVIDIA Jetson hardware and aggregated solutions at the PNY booth.
PNY’s platforms aggregate edge AI solutions tailored to Smart Cities & Spaces, incorporating Seeed’s Jetson hardware and software components to facilitate the efficient deployment and management of AI technologies.
3.Semtech: Booth 3-320 and 5-227
Check out our live tracker x Sidewalk demo at Semtech’s booth (3-320 and 5-227), which mirrors the demonstration we’ll be presenting at AWS’s booth.
4.Zephyr Project c/o The Linux Foundation: Booth 4-170
Visit us at Zephyr’s booth (4-170) to see our 2 products running Zephyr, including the SenseCAP T1000-S and Wio Terminal.
SenseCAP T1000-S, powered by Semtech LR1110 and Nordic‘s nRF52840, is a card-size tracker utilizing GNSS/Wi-Fi/Bluetooth for outdoor and indoor location tracking, supporting dual networks of both LoRaWAN® and Amazon Sidewalk. It boasts self-geo-adaptive capabilities, local data storage, and battery life for months. It’s equipped with temperature, light, and motion sensors, making it ideal for a variety of applications for location and status monitoring.
![](https://www.seeedstudio.com/blog/wp-content/uploads/2024/04/SENSECAPimage-1030x687.jpg)
Wio Terminal is an ATSAMD51-based microcontroller with both Bluetooth and Wi-Fi Wireless connectivity powered by Realtek RTL8720DN, compatible with Arduino and MicroPython. Currently, wireless connectivity is only supported by Arduino. More than just a single embedded functional module, Wio Terminal itself is integrated with a 2.4” LCD Screen, onboard IMU(LIS3DHTR), microphone, buzzer, microSD card slot, light sensor, infrared emitter(IR 940nm).On top of that, it also has two multifunctional Grove ports for Grove Ecosystem and 40 Raspberry pi compatible pin GPIO for more add-ons. All of these practical add-ons are carefully housed in a compact enclosure, making it an efficient and product-ready product. Equipped with Raspberry Pi 40-pin GPIO, it can be mounted to a Raspberry Pi as a slave device.
![](https://www.seeedstudio.com/blog/wp-content/uploads/2024/04/WIO-TERMINALimage-1030x773.jpg)
5.Raspberry Pi: Booth 3A-138
At Raspberry Pi’s booth (3A-138), we will showcase our products: reComputer R1000 and reTerminal DM.
The reComputer R1000 is a high-performance and cost-effective edge IoT controller based on Raspberry Pi solution. It features dual Ethernet interfaces and three isolated RS485 interfaces, supporting Modbus UDP/TCP and BACnet protocols, which makes it a perfect fit for smart buildings and energy management, such as controlling HVAC systems and other subsystems like lighting, sensors, and access control. With powerful IoT expansion capabilities, reComputer R1000 is integrated with various wireless transmission capabilities such as 4G, LoRa, Zigbee, Wi-Fi, and BLE through internal slots.
![](https://www.seeedstudio.com/blog/wp-content/uploads/2024/04/reComputer-R1000-1030x773.jpg)
reTerminal DM is a Panel PC, HMI, PLC, IIoT Gateway all-in-one device powered by Raspberry Pi CM4, with 10.1” IP65 front panel and rich industrial interfaces, and natively integrated with Node-RED and supports Raspberry Pi-based software ecosystem. This advanced version integrates a cameras and a PoE module, designed for much wider applications.
![](https://www.seeedstudio.com/blog/wp-content/uploads/2024/04/RETERMINAL-DMimage-1030x773.jpg)
6.ARM: Booth 4-504
At Arm‘s booth (4-504), you will be able to see a live demo with Seeed Grove Vision V2.
The demo shows you how Arm collaborates the ecosystem partners to empower every stage of ML developer workflow: from models to hardware. AI developers can now easily develop, test their ML applications with Arm Virtual Hardware and deploy them everywhere via Cortex-M based devices. Specificly, you will see the full process of how to develop an image classfication application(based on Baidu PaddlePaddle model) on Arm Virtual Hardware Corstone 300 platform and deploy it on Grove Vision AI V2 module.
![](https://www.seeedstudio.com/blog/wp-content/uploads/2024/04/v2-image-1030x773.jpg)
7.NetworkOptics: Booth 2-626
Network Optix (Nx) will have demos running on two sets of Seeed devices reRouter CM4 1432 and reComputer Orin.
For Demo 1, there will be multiple models deployed on reComputer Jetson Orin, including object detection and face detection. And you will be able to interact with various models onsite.
For Demo 2, you can train a model at the Network Optix booth with two behaviors (1) wearing Nx baseball cap and (2) not wearing the Nx baseball cap. The trained model will be imported in Nx cloud and then deployed on reRouter CM4 1432. Thus the camera will be able to detact whether the person in front of the camera wears the or does not wear the baseball cap.
8.The AI Hardware Show&Tell at EW2024
Meanwhile, we are organizing an AI Hardware Show & Tell on the evening of 10 April. We warmly invite you, our valued partners & customers to join us.
𝗛𝗶𝗴𝗵𝗹𝗶𝗴𝗵𝘁𝘀 𝗼𝗳 𝘁𝗵𝗶𝘀 𝗦𝗵𝗼𝘄 & 𝗧𝗲𝗹𝗹:
1. Grab drinks and mingle with like-minded people and tech-savvy gurus in the community and industry;
2. Connect with potential partners and customers to explore more collaboration opportunities;
3. Show your products, projects, and solutions that leverage open source and AI;
4. Get a first-hand touch of the rich collection of Seeed AI hardware and live demos.
We’re excited to connect with fellow innovators and technology enthusiasts at Embedded World 2024. If you’re attending the event, be sure to visit Booth 4-551 and our partners’ booths to to explore Seeed Studio’s open-source AI hardware solutions and experience live AI demos firsthand! We look forward to meeting you in person to discuss all things tech!