New Release: SenseCAP M4 Square-FluxNode and Helium
Since we released the SenseCAP M4 Square-FluxNode last December, we got lots of inquiries on a device to support dual Web 3.0 Apps. Today, we are excited to announce our latest release –SenseCAP Sqaure M4 Square-FluxNode and Helium, a powerful device designed to run multiple Web 3.0 Apps. The devices supports the no code seamless deployment of both a CUMULUS FluxNode and a Helium Light Hotspot, providing the community to set up scalable, decentralized computational network for Flux and miles of wireless Helium LoRaWAN network coverage meanwhile getting rewards for contributions to both netwoks.
Apart from this new device that supports both Flux and Helium, we’re also releasing a SenseCAP M4 Helium Kit for those who already own the SenseCAP M4 Sqaur-FluxNode to extend their FluxNode to be a Helium light hotspot.
CUMULUS FluxNodes powered by FluxOS FluxOS is a revolutionary second-layer operating system that allows hardened dockerized apps to run on Flux’s fully decentralized computational network, making it highly resilient to both system failure and outside attempts of censorship. SenseCAP M4 Square provides easy and friendly methods to deploy CUMULUS FluxNode with SenseCAP Hotspot App.
As a Helium light hotspot supporting the Helium LongFi network, it can provide miles of wireless network coverage and data transmission capacity for LoRaWAN® devices, which means it could help you build the local LoRaWAN network and develop various LoRaWAN applications at low cost while enjoying the benefits of being a part of the People’s Network. SenseCAP M4 Square is now providing US915 and EU868 versions with FCC and CE certificates.
Powered by SenseCAP Hotspot App, SenseCAP M4 Square provides an easy and friendly experience in deploying within 4 steps without a line of code. With SenseCAP’s one-stop cloud services (SenseCAP Hotspot App and SenseCAP Dashboard), we make it easy for anyone in the community to manage both FluxNode and Helium light hotspot and the entire lifecycle of devices (purchase devices, set up devices via Bluetooth, get comprehensive devices information, monitor device running status, contact tech support, and get the latest services and news provided) in just one app. Moreover, our dApp Center will be releasing more Web 3.0 applications in the future.
The SenseCAP Sqaure M4 Square-FluxNode and Helium is now available for pre-order in our official store at $359 (the 30 early birds can get it at $299). Run your FluxNode and Helium Light Hotspot on the same device now.
More to read:
2)Introduction of SenseCAP M2 Light Hotspot Service Package and How to Activate It