Running Klipper Screen on a reTerminal DM can provide several benefits, including the ability to monitor the printer’s status in real-time, the ability to control the printer remotely, and the ability to customize the printer’s settings. Additionally, Klipper Screen allows for the use of powerful features such as auto-tune, which can help to optimize the printer’s performance. Also possible to control multiple 3d printers all at once.