Tire Care device with machine learning based on Seeed Studio XIAO nRF52840 Sense
With Machine Learning it is possible to teach the device what is a “regular” break and what is a “tire wasting” break. How? Using an accelerometer. Seeed Studio Xiao nrf52840 Sense is powerful enough to run a machine learning model, has an on board accelerometer and fits a tiny enclosure.
Seeed Hardware: Seeed Studio XIAO nRF52840 Sense
Software: Arduino IDE、Edge Impulse
Industry: Industrial Site
Solution Deployment: Argentina
Background
The background of this project lies in addressing the issue of excessive braking, which can lead to significant tire wear and potential safety hazards. Historically, drivers have been known to engage in harsh braking habits, either due to inexperience, negligence, or simply being unaware of the consequences. This not only results in increased maintenance costs for vehicle owners but also contributes to environmental pollution through the release of harmful particulate matter from worn tires. By leveraging machine learning technology, the project aims to differentiate between regular and excessive braking, thereby promoting safer driving practices and reducing tire wear. To achieve this goal, the project utilizes the Seeed Studio Xiao nrf52840 Sense, a powerful device with an onboard accelerometer and compact size, making it suitable for vehicle integration. Ultimately, this project seeks to improve driving habits, lower vehicle operating costs, and contribute positively to environmental protection.
The Challenge
There are several challenges and potential difficulties that may arise while working on this project. First and foremost, developing a machine learning model capable of accurately differentiating between regular and excessive braking could be a complex task, as it requires a substantial amount of data collection and training to ensure the model’s effectiveness. Additionally, integrating the Seeed Studio Xiao nrf52840 Sense into a vehicle’s existing system might pose some technical challenges, particularly in terms of compatibility and ensuring that the device does not interfere with other vehicle components. Furthermore, user adoption might be a challenge, as convincing drivers to trust and rely on the system for improving their driving habits may require extensive marketing and education efforts. Lastly, ensuring the system’s reliability and robustness in various driving conditions and environments is crucial, as any false positives or negatives could potentially lead to safety concerns or ineffective results.
The Solution
For developing an accurate machine learning model, it is essential to collect a diverse and representative dataset that covers various driving scenarios, braking patterns, and conditions. This can be achieved by collaborating with a large group of drivers or using data from existing sources, such as vehicle telematics. Additionally, employing advanced machine learning techniques, such as deep learning and reinforcement learning, can help improve the model’s accuracy and performance.
To tackle the technical challenges of integrating the Seeed Studio Xiao nrf52840 Sense into a vehicle’s system, it is crucial to work closely with automotive engineers and experts who have experience in vehicle electronics and systems integration. They can provide valuable insights and guidance on ensuring compatibility and avoiding interference with other vehicle components.
To promote user adoption, it is essential to create a comprehensive marketing and education campaign that highlights the benefits of the system, such as improved driving habits, reduced tire wear, and environmental protection. This could include creating promotional materials, offering demonstrations, and providing user testimonials. Additionally, collaborating with driving schools, insurance companies, and fleet operators could help increase awareness and adoption of the system.
Ensuring the system’s reliability and robustness in various driving conditions and environments can be achieved through extensive testing and validation. This includes conducting tests in different weather conditions, road surfaces, and traffic situations to identify and address any potential issues or limitations. Furthermore, implementing rigorous quality control measures and continuously refining the system based on user feedback can help enhance its reliability and effectiveness.
The Results
Upon successful completion of this project, it could have a significant impact and offer substantial application value in various areas. Firstly, by accurately differentiating between regular and excessive braking, the system can help drivers improve their driving habits, leading to enhanced road safety and reduced chances of accidents. Secondly, by minimizing excessive braking, the system could contribute to decreased tire wear, resulting in lower maintenance costs for vehicle owners and reduced environmental pollution from worn tires.

Moreover, the system could be of particular interest to fleet operators and logistics companies, as it could help them monitor and improve their drivers’ performance, leading to increased efficiency and reduced operational costs. Additionally, insurance companies might also benefit from the system, as it could provide valuable data on driving habits, enabling them to offer personalized insurance plans based on individual driving behavior. Furthermore, the project could potentially pave the way for further research and development in the field of machine learning-based vehicle systems, opening up new possibilities for enhancing vehicle safety, performance, and efficiency.
More Info
- Learn more about products used: Seeed Studio XIAO nRF52840 Sense
- Discover Seeed Studio XIAO Series
- View and Download: System-on-Modules (SoM) User Manual