The EdgeLogix-RPi-1000 and EdgeBox-RPi-200 are powered by Raspberry Pi Compute Module 4. The powerful computing capability and rich software ecosystem of Raspberry Pi are the unique advantages of these two products. As a compact edge controller, the EdgeBox-RPi-200 is definitely the best choice for high performance requirements with low prices. EdgeLogix-RPi-1000, with its HMI addition function and rich industrial Ethernet interfaces, supports both cellular and LoRa, and is more suitable for high-demand industrial scenarios.