We Listen and Take Action #6: More Radar Sensors for Building Care Alert Solutions for Family

We got one very impressive feedback from our Wishing Well which shows the need for more smart home sensors in order to build a smart home solution for his/her grandma. 

We are really touched by this. Indeed, the miracle of smart home solutions has made life easier for many people, especially seniors.  Seeed is glad to help provide more smart home devices offer peace of mind for family members and caregivers providing assistance to elderly individuals.

First, we focus on falls detection. Falls are the major cause of accidents in the elderly population. In a real-life scenario, they have the potential to mitigate some of the adverse consequences of a fall. Specifically, fall detectors can have a direct impact on the reduction in the fear of falling and the rapid provision of assistance after a fall. 

Therefore, we released 24GHz mmWave Fall Detection Module

The other important aspect is the time the elderly remain lying on the floor after falling (long lie). This time is one of the key factors that determine the severity of a fall. Many older fallers are unable to get up again without assistance.  This is particularly critical if the person lives alone or loses consciousness after falling. They found that the long lie is a marker of weakness, illness, and social isolation and is associated with high mortality rates among the elderly. More than 20% of patients admitted to hospital because of a fall had been on the ground for an hour or more, and even if there was no direct injury from the fall, their morbidity rates within 6 months were very high. Robust fall detectors may have the potential to diminish this long lie. 

So, we offer 24GHz mmWave Human Static Presence Module. Compared to the traditional PIR sensor, the Human Static Presence Module has more sensitivity to human activities like standing, moving, and falling. And because the transmitting wave is millimeter-level, it will remain functioning even shelter block. Not like the PIR sensor short responding, the module keeps sensing people continuously which makes it quite useful during the living room, hotel, or even prison.

We also know that getting quality sleep is important for every person to get better physical health. Irregular sleep patterns may indicate the illness resulting in chronic depression, which makes the evaluation of the sleep cycle mandatory for a healthy body and mind. So we introduce Respiratory Sleep Radar Sensor(MR24BSD1) and Breathing and Heartbeat Module(MR60BHA1).

24GHz mmWave Sleep Breathing Monitoring Module

This radar module provides a fully total private and secure sensing environment, independently from other noisy influences. It is a useful privacy-protected, secure sensor radar system in smart home applications like sleep safety alarms, and sleep respiratory detection.

60GHz mmWave Breathing and Heartbeat Module

The MR60BHA1 60GHz radar module applies FMCW detected theory to implement simultaneous personal breathing rate and heart rate detention in high accuracy, providing a fully total private and secure environment, independently from other noisy influences. It is a standard biotic radar system in consumer electronics, healthcare as well as industrial applications.

We care about every little detail when it comes to providing better products and services for our customers. If you think there are other sensors you want Seeed to provide, just let us know on Wishing Well. We check the wishing well every day and will get back to your feedback quickly. Your suggestion could lead to improvements that benefit everyone. 

✨We Listen and Take Action

We Listen and Take Action #1: Delivery Charge Cut Down by Half, Less Than $5 Shipping All over the World.

We Listen and Take Action #2: Let us Hear Your Voices!

We Listen and Take Action #3: LoRa-E5 Modules are Available in Tape/Reel Packaging

We Listen and Take Action #4: Be an Advocate of Open Source Development with Project Sharing

We Listen and Take Action #5: New FedEx Shipping Option Live, Especially for Orders without Batteries

We Listen and Take Action #6: More Radar Sensors for Building Care Alert Solutions for Family

We Listen and Take Action #7: Smoother and Richer Search Experience Now Available

We Listen and Take Action #8: New UK Warehouse Open Live

We Listen and Take Action #9: A sense of engagement, Seeed builds the Wio-E5 CAN Development Kit together with the community

We Listen and Take Action #10: Mid-year ‘Share2Get’ month-long campaign in full swing

We Listen and Take Action #11: XIAO RP2040 Global Free Shipping From Seeed + Changes Of Small Parcel Limit? Yes. Get Excited!

We Listen and Take Action #12: Seeed New EU Warehouse Now Open in Germany!

We Listen and Take Action #13: Accelerate Delivery Time by Over 70%! EU Warehouse Started Supporting A New Shipping Method Now.

About Author

Calendar

2022 年 4 月
 123
45678910
11121314151617
18192021222324
252627282930