SLAMTEC RPLiDAR S2: New generation TOF radar with ultra-high standard sampling and precision for industrial scenarios
Compared with other series of laser scanners, we have introduced RPLIDAR from SLAMTEC with RPLIDAR S1 is more stable in detecting long-distance objects and direct-light objects can achieve ideal mapping effects within a 40-meter ranging radius for indoor and outdoor environments and are able to be expanded to more usage scenarios.
![](https://www.seeedstudio.com/blog/wp-content/uploads/2021/10/image-14.png)
Aiming at adapting to more application scenarios and more industrial requirment, SLAMTEC team has upgraded the RPLIDAR produce line with the second-generation TOF radar, RPLIDAR S2. It has improved hardware performance and optimized software algorithms. From the perspective of product parameters, RPLIDAR S2 has obvious advantages in terms of the sampling frequency, angular resolution, and product size.
Features:
- High-speed laser ranging sampling capability of 32,000 times per second
- Non-contact energy and signal transmission technology
- Reliable and stable operation for a long time
- Coverage area with a radius of 30 meters on a two-dimensional plane
- 360° omnidirectional laser ranging scanning
- Excellent application in both indoor and outdoor environments
- Built-in speed detection and adaptive system
- Cost reduction because there is no need to provide a complex power supply system
- The emitted laser power complies with IEC-60825 Class 1 human eye safety level
Compared with RPLIDAR S1, RPLIDAR S2 is a quasi-industrial TOF radar with an IP65 protection level. It has more stable and reliable ranging performance when detecting long-distance objects, switching between black and white objects, and strong direct light objects. At the same time, the compact size and excellent angular resolution also make it more widely used. RPLIDAR S2 adopts laser time-of-flight ranging technology, coupled with the high-speed laser acquisition and processing mechanism developed by SLAMTEC, which can perform 32,000 ranging actions per second. It uses non-contact energy and signal transmission technology, overcomes the life limitation of traditional lidar, and can operate reliably and stably for a long time.
RPLIDAR S2 DTOF time-of-flight ranging technology uses DTOF (Direct Time of Flight) time-of-flight ranging technology to ensure that the measurement accuracy of lidar is excellent at any distance, and it can effectively detect low reflectance, specular reflection and even high transmittance.
DTOF time-of-flight ranging technology
![](https://www.seeedstudio.com/blog/wp-content/uploads/2021/10/image-15.png)
Perfect compact size to embedded to Robot
The height of the scanning area on the top of the radar is only 18mm, which is small and easy to be embedded, which can greatly reduce the opening height of the robot radar area. When RPLIDAR S2 is installed in the robot, the overall appearance design of the robot will not be affected.
![](https://www.seeedstudio.com/blog/wp-content/uploads/2021/10/image-16.png)
RPLIDAR product line specification comparision
Measurement Performance | Distance Range | Measurement Resolution | Angular Resolution | Sample Rate | Working Environment |
RPLIDAR A1M8 | 0.15m -12m | <0.5 mm | ≤1° | 2000 – 8000 Hz | Indoor |
<1% of actual distance * | |||||
RPLIDAR A2M6 | 0.2m – 18m | <0.5 mm | ≤0.9° | 2000 – 8000 Hz | Indoor |
<1% of actual distance * | |||||
RPLIDAR A2M8 | 0.15m -12m | <0.5 mm | ≤0.9° | 2000 – 8000 Hz | Indoor |
<1% of actual distance * | |||||
RPLIDAR A3M1 | White object: 25 meters | 0.225° | 16 kHz or 10 kHz | Indoor & Outdoor | |
Dark object: 10 meters | |||||
RPLIDAR S1 | White Objects: 40m | 3cm | 0.313°-0.587° | 9200 Hz | Indoor& Outdoor |
Black Object: 10m | |||||
SLAMTEC MAPPER M1M1 | 20m | 5cm | 7000 Hz | Indoor & Outdoor | |
RPLiDAR S2 | White object: 0.05~30 meters | 3cm | 0.12° | 32KHz | Indoor & Outdoor with IP65 protection |
Black object: 0.05~10 meters |
Application Scenarios
- The RPLIDAR can be used in the following application scenarios:
- General robot navigation and localization
- Environment scanning and 3D re-modeling
- Service robot or industrial robot working for long hours
- Home service /cleaning robot navigation and localization
- General simultaneous localization and mapping (SLAM)
- Smart toy’s localization and obstacle avoidance
![](https://www.seeedstudio.com/blog/wp-content/uploads/2021/10/image-17-1030x250.png)
Framegrabber plug-in and RoboStudio SDK
In order to facilitate users to use RPLIDAR S2 in product development and speed up the user’s development cycle, Silan provides the Framegrabber plug-in in RoboStudio for testing and debugging and provides SDK under Windows, x86 Linux, and Arm Linux. Download here: https://download.slamtec.com/api/download/rplidar-sdk/1.11.0?lang=netural
![](https://www.seeedstudio.com/blog/wp-content/uploads/2021/10/image-18.png)
You wil know find more about RPLIDAR and Slamec technology in the following articles:
- All you need to know about Slamtec RPLIDAR, MAPPER and Slamware
- RPLIDAR and ROS programming- The Best Way to Build Robot
- Introducing RPLIDAR S1 – Portable TOF 360° Laser Range Scanner
- Installing ROS Melodic on Raspberry Pi 4 and RPLIDAR A1M8
- Add a Laser Scanner to your Robot – the key to enabling SLAM