#New product idea# Grove Base Plate for better showing your project and prototype assembling
![](https://blog.seeedstudio.com/wp-content/uploads/2020/10/微信图片_20201028110520-1030x773.jpg)
Thanks to our Seeed Ranger @Reivilo for putting up this original good idea on Seeed Forum.
The idea is that we should have a base plate to hold the Grove devices and main boards. It would be very nice to assemble all components together in a neat and clear way, especially for easy testing and better showing your prototype.
![](https://blog.seeedstudio.com/wp-content/uploads/2020/10/image-40.png)
@Reivilo is very kind to also provide with a sample design, which is a base plate with φ2mm holes for M2 screws of 10mm hole distance.
![](https://blog.seeedstudio.com/wp-content/uploads/2020/10/image-41.png)
Considering to be better compatible with most of the main boards which have M3 mounting holes, we designed a board that have holes of both M2 and M3 sizes.
At the same time, for better accomadating and hiding the Grove cables, there are also bigger holes for Grove connector to go through, making your design of prototype more elegant.
![](https://blog.seeedstudio.com/wp-content/uploads/2020/10/image-42.png)
![](https://blog.seeedstudio.com/wp-content/uploads/2020/10/微信图片_20201028110524-1030x773.jpg)
How do you like this idea and design? Welcome to the Forum and tell us your suggestions~ If you do like it, let’s make it come to life together~