DeskPi Pro Set-top Box For Raspberry Pi 4 now available at Seeed

Last week DeskPi Pro Set-top Box with aluminum and NUC design style just arrived at Seeed and we got a lot of positive feedback from customers said they really want it in hands! Now DeskPi Pro Set-top Box For Raspberry Pi 4 is available for pre-order. The first batch will be shipped on Oct 15, 2020.
If you are looking for more storage attach on your Raspberry Pi 4? DeskPi Pro will be a nice choice as it supports 2.5″ HDD/SSD drive in the case. The PCB inside has a 7+15 pin SATA connector inside where you can connect a 2.5 inch HDD or an SSD to your Raspberry Pi 4 via a USB 3.0 connection
This NUC style aluminum alloy case provides better protection and has excellent cooling as well with the built-in ICE Tower Cooler and carefully cut-out air vents. Also, there are 2 Full-Size HDMI ports with 4K support on the case which are converted from the micro-HDMI ports on the Raspberry Pi 4.
Do you still remember ICE Tower Cooler?

Tower structure, 5mm copper tube, multi-layer heat sinks, 7 blades powerful fan, all the above combinations make this super radiator for Raspberry Pi. In the case of overclocking, it can reduce the temperature of the Raspberry Pi from 80℃ to 40℃. We also found that Raspberry Pi 4 has a large amount of heat. with the help of this super fan, the powerful performance of the Raspberry Pi 4 will be fully released.
At Seeed, we are keeping sourcing awesome different Raspberry Pi 4 cases, you can find more through the blog Best 11 Raspberry Pi 4 Cases Selection and Best Accessories Guide for Raspberry Pi 4. Hope our guides will help you get the most suitable case and accessories for Raspberry Pi 4.
Hardware Overview
.png)
- 1. Low Profile ICE Tower Cooler (inside the case)
- 2. Micro-SD Card Slot
- 3. USB 2.0 HOST
- 4. USB 2.0 HOST
- 5. Safe Power/ Reset Button

- 6. Type-C (PD 2.0 & QC 3.0) Input
- 7. Full-Size HDMI Port, Support 4K
- 8. Full-Size HDMI Port, Support 4K
- 9. 3.5mm Audio & AV Jack
- 10. 2.5 inch HDD/SSD expansion (inside the case)
- 11. USB 3.0
Feel free to let us know what else cases and accessories are you looking for Raspberry Pi 4. We will carefully listen to the community and take action! Find us on Twitter @seeedstudio or Forum!