New data-driven method to control the movement of multiple Crazyflie by Caltech: Machine Learning Helps Robot Swarms Coordinate
The following content firstly appeared on the news of Caltech, Machine Learning Helps Robot Swarms Coordinate
![](https://blog.seeedstudio.com/wp-content/uploads/2020/07/image-28-1030x446.png)
We contacted postdoctoral scholar Wolfgang Hönig to learn more about the project. It is glad to know the project was using Crazyflie. Videos and projects used Crazyflie 2.X, with a mix of the previous version Crazyflie 2.0 and the latest version of Crazyflie 2.1. Wolfgang said that Crazyflie 2.1 was in particular advantageous for the Neural-Swarm project due to the lower noise of its IMU sensor. The “large” drones in the Neural-Swarm project use Crazyflie 2.1 as control boards, but different motors + frames.
Engineers at Caltech have designed a new data-driven method to control the movement of multiple robots through cluttered, unmapped spaces, so they do not run into one another.
Multi-robot motion coordination is a fundamental robotics problem with wide-ranging applications that range from urban search and rescue to the control of fleets of self-driving cars to formation-flying in cluttered environments. Two key challenges make multi-robot coordination difficult: first, robots moving in new environments must make split-second decisions about their trajectories despite having incomplete data about their future path; second, the presence of larger numbers of robots in an environment makes their interactions increasingly complex (and more prone to collisions).
To overcome these challenges, Soon-Jo Chung, Bren Professor of Aerospace, and Yisong Yue, professor of computing and mathematical sciences, along with Caltech graduate student Benjamin Rivière (MS ’18), postdoctoral scholar Wolfgang Hönig, and graduate student Guanya Shi, developed a multi-robot motion-planning algorithm called “Global-to-Local Safe Autonomy Synthesis,” or GLAS, which imitates a complete-information planner with only local information, and “Neural-Swarm,” a swarm-tracking controller augmented to learn complex aerodynamic interactions in close-proximity flight.
“Our work shows some promising results to overcome the safety, robustness, and scalability issues of conventional black-box artificial intelligence (AI) approaches for swarm motion planning with GLAS and close-proximity control for multiple drones using Neural-Swarm,” says Chung.
When GLAS and Neural-Swarm are used, a robot does not require a complete and comprehensive picture of the environment that it is moving through, or of the path its fellow robots intend to take. Instead, robots learn how to navigate through a space on the fly, and incorporate new information as they go into a “learned model” for movement. Since each robot in a swarm only requires information about its local surroundings, decentralized computation can be done; in essence, each robot “thinks” for itself, which makes it easier to scale up the size of the swarm.
“These projects demonstrate the potential of integrating modern machine-learning methods into multi-agent planning and control, and also reveal exciting new directions for machine-learning research,” says Yue.
To test their new systems, Chung’s and Yue’s teams implemented GLAS and Neural-Swarm on quadcopter swarms of up to 16 drones and flew them in the open-air drone arena at Caltech’s Center for Autonomous Systems and Technologies (CAST). The teams found that GLAS could outperform the current state-of-the-art multi-robot motion-planning algorithm by 20 percent in a wide range of cases. Meanwhile, Neural-Swarm significantly outperformed a commercial controller that cannot consider aerodynamic interactions; tracking errors, a key metric in how the drones orient themselves and track desired positions in three-dimensional space, were up to four times smaller when the new controller was used.
Their research appears in two recently published studies. “GLAS: Global-to-Local Safe Autonomy Synthesis for Multi-Robot Motion Planning with End-to-End Learning” was published in IEEE Robotics and Automation Letters on May 11 by Chung, Yue, Rivière, and Hönig. “Neural-Swarm: Decentralized Close-Proximity Multirotor Control Using Learned Interactions” was published in Proceedings of IEEE International Conference on Robotics and Automation on June 1 by Chung, Yue, Shi, and Hönig. This research was supported by the Raytheon Company; CAST; and JPL, which Caltech manages for NASA.
Resources
Machine Learning Helps Robot Swarms Coordinate – Caltech News July 13, 2020