Wio Terminal Community Project Collection

Wio Terminal is an ATSAMD51-based microcontroller with wireless connectivity supported by Realtek RTL8720DN. It is equipped with a 2.4” LCD Screen, onboard IMU(LIS3DHTR), Microphone, Buzzer, microSD card slot, Light sensor, and Infrared Emitter(IR 940nm).

Since the release of Wio Terminal, we have seen many creative projects from the community. We collected various projects in this post and hope some of them will inspire you!


October 22th, 2020 Updated: high accuracy Wio terminal attitude indicator by @FenyiShi


October 15th, 2020 Updated: Running the Adafruit Uncanny Eyes on Wio Terminal

October 15th, 2020 Updated: Wio Terminal Weather station using BME280 and PlatformIO by @survivingwithan

October 15th, 2020 Updated: Drawing Japanese in Wio Terminal using LovyanGFX v0.2.3 by @lovyan03


September 27th, 2020 Updated: Playing Wio Terminal’s BLE with Blynk and RGB strips!

check the full tutorial here!

https://twitter.com/Ansonnh/status/1310063708903677952

September 27th, 2020 Updated: Controlling servo whilst reading accelerator readings on Wio Terminal using BLE on Blynk!

https://twitter.com/Ansonnh/status/1309445647246831616

September 27th, 2020 Updated: Hack Your Car With Wio Terminal and CAN Bus by Longan Labs

图像

September 27th, 2020 Updated: LCARS SmartHome SmartSensor Using WioTerminal by @KeHo_Software

https://twitter.com/KeHo_Software/status/1308085894356836352

September 10th, 2020 Updated: 12-key Keyboard Using Wio Terminal by @carcon999


September 10th, 2020 Updated: Air quality Monitoring Station with Wio Terminal by Salman Faris

The Air Quality Terminal can be used as an indoor air quality meter to monitor VOCs, CO, NO2, C2H5CH, Temp and Humidity.

Air quality Monitoring Station with Wio Terminal

August 27th, 2020 Updated: WiFi Analyzer that can also scan 5 GHz Network by @moononournation


August 20th, 2020 Updated: Create A Retro Game in ArduPy for Wio Terminal by @ezContents


August 20th, 2020 Updated: How to Make a Contactless Temperature Monitor By Rei Vilo

Contactless Temperature Monitor

July 30, 2020 Updated: pycalculator by CircuitPython on WioTerminal!


July 30, 2020 Updated: Connect Wio Terminal with BeagleBone Green and make an automotive dashboard


July 30, 2020 Updated: Egg Timer with Pictures


July 23, 2020 Updated: Wio Terminal-based Easy Smart Home Automation System


July 23, 2020 Updated: Playing Big Buck Bunny on WioTerminal with Raspberry Pi 4

July 23, 2020 Updated: Bling-Bling DIY Keyboard


July 23, 2020 Updated: Play SuperMario Retro Game on Wio Terminal

July 23, 2020 Updated: Wio Terminal-Based Environment Monitor System

https://twitter.com/kamiya_owl/status/1284149344556351489

July 16, 2020 Updated: ExtFlashLoader v0.1.2, A Library to Access External Flash in Wio Terminal and A Sample Sketch to Enable Loading Applications from TF Card


July 9, 2020 Updated: Use Wio Terminal to Build an Open Source USB Monitor


July 2, 2020 Updated: DIY mini Blinking keyboard using Wio Terminal & Original Keycaps


July 2, 2020 Updated: A comparison of TFT_eSPI & LovyanGFX


June 18th, 2020 Updated: Made the Main Character of the Default Game Stronger and Made it Easier to Play


June 18th, 2020 Updated: The 3D-printed Case for this Artificial Nose is now Finished!


June 11th, 2020 Updated: Run LovyanGFX, a High-Speed GUI(Graphical User Interface) on Wio Terminal


June 11th, 2020 Updated: Turn Wio Terminal into an Oscilloscope


June 11th, 2020 Updated: DIY USB Keyboard

https://twitter.com/carcon999/status/1266718037282926592

June 11th, 2020 Updated: Check this 3D printed enclosure for the artificial nose project!

Artificial Nose that can Discern Different Kinds of Rum or Scotch


Projects by Homemadegarbage

Thanks homemadegarbage (twitter: @H0meMadeGarbage) for sharing the below projects in his blog Wio Terminal を使ってみた, and Wio Terminal でパルスオキシメータを制作. We have got authorized from him and translated his guides to the English version. Let’s have a look!

TV Remote Controller

For detailed tutorial, check here: Three Entry-level Demos Help You Get Started with Wio Terminal Quickly

Pulse Oximeter

There is also a guide about How to Build a Cost-effective Pulse Oximeter with Wio Terminal and MAX30105 Sensor.


Weather Forecast


Run TinyGO on Wio Terminal


Use LovyanGFX, a High-Performance Graphics library on Wio Terminal


Tipsy Glass


Gaming

https://www.instagram.com/p/CAQJyWJg-b0/?igshid=1p5b7eldalacu

Printer


GPS Navigator


Water Level Detector


Machine Learning on Wio Terminal

A non-invasive solution for hot flashes during menopause using machine learning made by Naveen. Learn more at here.


If you also make some awesome projects using Wio Terminal, don’t hesitate to @seeedstudio on Twitter or leave a comment!

About Author

Calendar

May 2020
M T W T F S S
 123
45678910
11121314151617
18192021222324
25262728293031