New Product Idea: Functional Expansion Board​ for Seeeduino XIAO

Grove Shield for SeeeduinoXIAO with 25*58mm slim rectangular shape is about to enter mass production period, and hopefully could see it on the Bazaar in June. 

Besides a normally Grove expansion shield for SeeeduinoXIAO, how do you like to have a functional expansion board for SeeeduinoXIAO?

We tried to design this two version, which do you prefer? Or you have better ideas?

Do not hesitate to tell us on the Forum:

#Product Idea# SeeeduinoXIAO Functional Expansion Board Design – Waiting for Inputs  

Waiting for you valuable opinion…

About Author

2 thoughts on “New Product Idea: Functional Expansion Board​ for Seeeduino XIAO

    1. Hi,Nicho. Infrared reflection sensor is a sensor for distance detection. An on board intergrated infrared reflection sensor could make you easily to develop many project associated with distance, and you could have the project size more compact by not add anther IR module.

      Recently we developed a pocket distance alarm demo, which will make sure others stay one meter away during the outbreak, and the ToF we used could be replaced with IR sensor also, see follows if interested:
      Use Seeeduino Xiao to make a Pocket Distance Alarm – making sure others stay one meter away https://blog.seeedstudio.com/blog/2020/04/03/use-seeeduino-xiao-to-make-a-pocket-distance-alarm-making-sure-others-stay-one-meter-away/

Comments are closed.

Calendar

May 2020
M T W T F S S
 123
45678910
11121314151617
18192021222324
25262728293031