Prototype with Coral Intelligence; Leverage the Power of Google’s Edge TPU at a New Lower Price
Coral is a division of Google, that helps you build intelligent ideas with their platform for local AI. Their Dev Board features Google’s Edge TPU chip for fast ML inferencing on the device. Now there are price drops on the Coral USB Accelerator, Dev Board, and Camera Module beginning from May 1st.
Google Coral USB Accelerator now dropped a new price of $59.99 (was $74.99)
The Coral USB Accelerator brings powerful ML inferencing capabilities to existing Linux systems.
Featuring the Edge TPU — a small ASIC designed and built by Google— the USB Accelerator provides high-performance ML inferencing with a low power cost over a USB 3.0 interface. For example, it can execute state-of-the-art mobile vision models such as MobileNet v2 at 100+ fps, in a power-efficient manner. This allows you to add fast ML inferencing to your embedded AI devices in a power-efficient and privacy-preserving way.

Coral Dev Board now dropped a new price of $129.00 (was $149.99)
The Coral Dev Board is a single-board computer with a removable system-on-module (SOM) that contains eMMC, SOC, wireless radios, and Google’s Edge TPU. It’s perfect for IoT devices and other embedded systems that demand fast on-device ML inferencing.

Coral Camera Module now dropped a new price of $19.99.(was $24.99)
The Coral Camera is a 5MP camera designed for use with the Coral Dev Board, providing input for computer vision use cases. The camera attaches to the Coral Dev Board’s MIPI CSI interface with a 24-pin FFC.
- ISP function: Automatic exposure control (AEC), automatic white balance (AWB), automatic band filter (ABF), automatic 50/60 Hz lumination, automatic blacklevel calibration (ABLC).
- Image quality control: color saturation, hue, gamma, sharpness, lens correction, defective pixel canceling, and noise canceling.
- Support autofocus control (AFC) with embedded AF VCM Driver.
- For more information about the sensor, read about the Omnivision SOC.