Update of PCIe to SATA RAID Module for the ODYSSEY – X86J4105
This week we have received the first batch sample of PCIe to SATA RAID for the ODYSSEY – X86. We have tested it and everything works fine.

You might wonder what controller we are using on the module, and here is it: ASM1062 from ASMedia, it can bridge PCI Express Gen2 x2 to two ports of Serial ATA 6Gps, enables Serial ATA PHY up to 6Gps high-speed interface, supports SRIS (Separate Refclk Independent SSC) function, complies with Serial ATA Revision 3.2 Specification.

Another thing you might have noticed is that we chose a horizontal SATA port for the design so that it will be more suitable to put in the re_computer case. Can’t wait to make a NAS with it.

If you have any questions or doubt for the ODYSSEY – X86 or the re_computer case, welcome to discuss with us in our forum.