Wio Terminal Update: Build An Affordable IR Thermal Imaging Camera

Now you can make an affordable thermal camera with Wio Terminal and Grove – Infrared Temperature Sensor Array (AMG8833). The total cost for all the components is less than $80 and you can get a low-cost FLIR™ like a thermal imagining camera with ease.

What is infrared, and how to “see” and use it

To start with, let’s take a quick look at infrared. Infrared (IR), or infrared light, is electromagnetic radiation (EMR) with longer wavelengths compared with visible light, which makes it invisible to the human eye in general condition. Most of the thermal radiation emitted by objects near room temperature is infrared. (Ref: Wikipedia)

Human eyes cannot “see” Infrared light since it has longer wavelengths than visible light, but a thermal infrared camera can provide a simple solution. It can detect infrared energy and convert it into a picture with different colors, showing the temperature of detected items.

Below is some typical application of IR thermal imaging camera:

  • Non-contact temperature measurements in medical care
  • Fire prevention systems
  • Intrusion/Movement detection
  • Presence detection / Person localization
  • Sensing elements for smart home

Build a DIY IR Thermal Imaging Camera

To set you back a little, the resolution of the Grove – Infrared Temperature Sensor Array (AMG8833) is only 8 x 8 (64 Pixels), which in some cases is good enough. So Linear Interpolation is used in the code to expand to 70 x 70 (4900 Pixels) for a much better indication.

This demo is inspired by Kris Kasprzak’s video. Several modifications were made to make it compatible with Wio Terminal and Grove – Infrared Temperature Sensor Array (AMG8833). Most Graphics are now first drawn to TFT LCD Sprites first to improve overall performance and faster frame rate. We also added a crosshair in the middle of the screen and showing the temperature at the crosshair. By the way, you can turn on or off the reference line on the screen by clicking the right button upon Wio Terminal.

With reference line
Without reference line

Hardware Requirement

Note: The Wio Terminal and battery chassis used in this post are demos for testing, so their outlook is slightly different from the pictures at the right. For example, the button of Wio Terminal should be blue, and the enclosure of the battery chassis should be white.

Software Requirement

  • Install the LCD screen Library Seeed_Arduino_LCD, please visit Wio Terminal LCD for more information.
  • Visit the Seeed_AMG8833 repositories and download the entire repo to your local drive.
    • Now, the Seeed_AMG8833 library can be installed to the Arduino IDE. Open the Arduino IDE, and click sketch -> Include Library -> Add .ZIP Library, and choose the Seeed_AMG8833 file that you’ve have just downloaded.

Setup Instructions

  • Plugin the Grove – Infrared Temperature Sensor Array (AMG8833) to the Grove I2C Interface of Wio Terminal.
  • Download the Complete code here or copy the code at the end of this page.
  • Upload the code.

Now you can turn on Wio Terminal and have a try of your new IR thermal imaging camera!

Explore More at Our Github & Forum

Want to know more about Wio Terminal? Our brand-new Forum has been released and is waiting for you to join our discussion! Feel free to post your questions or any technical issue about Wio Terminal at our forum. We can’t wait to hear your voices and welcome all suggestions!

In case of anyone having no idea of what Wio Terminal is, let’s take a look at it together!

A Brief Introduction of Wio Terminal

Wio Terminal is a simple and tiny device to build I/O with the physical world. It is an ATSAMD51-based Dev. board with wireless connectivity supported by Realtek RTL8720DN.


Complete Code

Note: To boost up performance and frame rate of this IR Thermal Imaging Camera, you can boost the Wio Terminal CPU Speed to 200MHz. Select Tools -> CPU Speed -> 200MHz(Overclock)

/*

  This program is for upsizing an 8 x 8 array of thermal camera readings
  it will size up by 10x and display to a 240 x 320
  interpolation is linear and "good enough" given the display is a 5-6-5 color palet
  Total final array is an array of 70 x 70 of internal points only

  Revisions
  1.0     Kasprzak      Initial code
  1.1     Anson(Seeed Studio)  Adapted to Wio Terminal with Grove - Infrared Sensor(AMG8833)

*/

#include <Seeed_AMG8833_driver.h>
#include <TFT_eSPI.h>                // Include the graphics library (this includes the sprite functions)  

TFT_eSPI    tft = TFT_eSPI(); 
TFT_eSprite Display = TFT_eSprite(&tft);  // Create Sprite object "img" with pointer to "tft" object
// the pointer is used by pushSprite() to push it onto the TFT

unsigned long CurTime;

uint16_t TheColor;
// start with some initial colors
uint16_t MinTemp = 25;
uint16_t MaxTemp = 35;

// variables for interpolated colors
byte red, green, blue;

// variables for row/column interpolation
byte i, j, k, row, col, incr;
float intPoint, val, a, b, c, d, ii;
byte aLow, aHigh;

// size of a display "pixel"
byte BoxWidth = 3;
byte BoxHeight = 3;

int x, y;
char buf[20];

// variable to toggle the display grid
int ShowGrid = -1;

// array for the 8 x 8 measured pixels
float pixels[64];

// array for the interpolated array
float HDTemp[80][80];

// create the camara object
AMG8833 ThermalSensor;

//Toggle the grid on and off
void toggleGrid() {
  ShowGrid = ShowGrid *-1;
  Display.fillRect(15, 15, 210, 210, TFT_BLACK);
  yield();
}

void setup() {
  Serial.begin(115200);

  // start the display and set the background to black
  tft.begin();
  tft.fillScreen(TFT_BLACK);

  //Interrupt to toggle Gird on and off
  pinMode(WIO_KEY_A, INPUT);
  attachInterrupt(digitalPinToInterrupt(WIO_KEY_A), toggleGrid, FALLING);

  // set display rotation (you may need to change to 0 depending on your display
  tft.setRotation(3);

  // show a splash screen

  tft.setCursor(20, 20);
  tft.setTextColor(TFT_BLUE, TFT_BLACK);
  tft.print("Thermal ");

  tft.setTextColor(TFT_RED, TFT_BLACK);
  tft.print("Camera");

  // let sensor boot up
  bool status = ThermalSensor.init();
  delay(100);

  if (!status) {
      Serial.print("Failed to initalized AMG8833");
  }

  // read the camera for initial testing
  ThermalSensor.read_pixel_temperature(pixels);

  // check status and display results
  if (pixels[0] < 0) {
    while (1) {
      tft.setCursor(20, 40);
      tft.setTextColor(TFT_RED, TFT_BLACK);
      tft.print("Readings: FAIL");
      delay(500);
    }
  }
  else {
    tft.setCursor(20, 40);
    tft.setTextColor(TFT_GREEN, TFT_BLACK);
    tft.print("Readings: OK");
    delay(2000);
  }

  tft.fillScreen(TFT_BLACK);

  Display.createSprite(TFT_HEIGHT, TFT_WIDTH);
  Display.fillSprite(TFT_BLACK); 

  // get the cutoff points for the color interpolation routines
  // note this function called when the temp scale is changed
  Getabcd();

  // draw a legend with the scale that matches the sensors max and min
  DrawLegend();

}

void loop() {  
  CurTime = millis();

  // draw a large white border for the temperature area
  Display.fillRect(10, 10, 220, 220, TFT_WHITE);

  // read the sensor
  ThermalSensor.read_pixel_temperature(pixels);

  // now that we have an 8 x 8 sensor array
  // interpolate to get a bigger screen
  // interpolate the 8 rows (interpolate the 70 column points between the 8 sensor pixels first)
  for (row = 0; row < 8; row ++) {
    for (col = 0; col < 70; col ++) {
      // get the first array point, then the next
      // also need to bump by 8 for the subsequent rows
      aLow =  col / 10 + (row * 8);
      aHigh = (col / 10) + 1 + (row * 8);
      // get the amount to interpolate for each of the 10 columns
      // here were doing simple linear interpolation mainly to keep performace high and
      // display is 5-6-5 color palet so fancy interpolation will get lost in low color depth
      intPoint =   (( pixels[aHigh] - pixels[aLow] ) / 10.0 );
      // determine how much to bump each column (basically 0-9)
      incr = col % 10;
      // find the interpolated value
      val = (intPoint * incr ) +  pixels[aLow];
      // store in the 70 x 70 array
      // since display is pointing away, reverse row to transpose row data
      HDTemp[ (7 - row) * 10]
= val; } } // now that we have raw data with 70 columns // interpolate each of the 70 columns // forget Arduino..no where near fast enough..Teensy at > 72 mhz is the starting point for (col = 0; col < 70; col ++) { for (row = 0; row < 70; row ++) { // get the first array point, then the next // also need to bump by 8 for the subsequent cols aLow = (row / 10 ) * 10; aHigh = aLow + 10; // get the amount to interpolate for each of the 10 columns // here were doing simple linear interpolation mainly to keep performace high and // display is 5-6-5 color palet so fancy interpolation will get lost in low color depth intPoint = (( HDTemp[aHigh]
- HDTemp[aLow]
) / 10.0 ); // determine how much to bump each column (basically 0-9) incr = row % 10; // find the interpolated value val = (intPoint * incr ) + HDTemp[aLow]
; // store in the 70 x 70 array HDTemp[ row ]
= val; } } //display the 70 x 70 array DisplayGradient(); //Crosshair in the middle of the screen Display.drawCircle(115, 115, 5, TFT_WHITE); Display.drawFastVLine(115, 105, 20, TFT_WHITE); Display.drawFastHLine(105, 115, 20, TFT_WHITE); //Push the Sprite to the screen Display.pushSprite(0, 0); //Displaying the temp at the middle of the Screen tft.setRotation(3); tft.setTextColor(TFT_WHITE); tft.drawFloat(HDTemp[35][35], 2, 90, 20); //Uncomment this to print out frame rate Serial.print("Frame rate: "); Serial.println(1/(0.001*(millis() - CurTime))); } // function to display the results void DisplayGradient() { tft.setRotation(4); // rip through 70 rows for (row = 0; row < 70; row ++) { // fast way to draw a non-flicker grid--just make every 10 pixels 2x2 as opposed to 3x3 // drawing lines after the grid will just flicker too much if (ShowGrid < 0) { BoxWidth = 3; } else { if ((row % 10 == 9) ) { BoxWidth = 2; } else { BoxWidth = 3; } } // then rip through each 70 cols for (col = 0; col < 70; col++) { // fast way to draw a non-flicker grid--just make every 10 pixels 2x2 as opposed to 3x3 if (ShowGrid < 0) { BoxHeight = 3; } else { if ( (col % 10 == 9)) { BoxHeight = 2; } else { BoxHeight = 3; } } // finally we can draw each the 70 x 70 points, note the call to get interpolated color Display.fillRect((row * 3) + 15, (col * 3) + 15, BoxWidth, BoxHeight, GetColor(HDTemp[row]
)); } } } // my fast yet effective color interpolation routine uint16_t GetColor(float val) { /* pass in value and figure out R G B several published ways to do this I basically graphed R G B and developed simple linear equations again a 5-6-5 color display will not need accurate temp to R G B color calculation equations based on http://web-tech.ga-usa.com/2012/05/creating-a-custom-hot-to-cold-temperature-color-gradient-for-use-with-rrdtool/index.html */ red = constrain(255.0 / (c - b) * val - ((b * 255.0) / (c - b)), 0, 255); if ((val > MinTemp) & (val < a)) { green = constrain(255.0 / (a - MinTemp) * val - (255.0 * MinTemp) / (a - MinTemp), 0, 255); } else if ((val >= a) & (val <= c)) { green = 255; } else if (val > c) { green = constrain(255.0 / (c - d) * val - (d * 255.0) / (c - d), 0, 255); } else if ((val > d) | (val < a)) { green = 0; } if (val <= b) { blue = constrain(255.0 / (a - b) * val - (255.0 * b) / (a - b), 0, 255); } else if ((val > b) & (val <= d)) { blue = 0; } else if (val > d) { blue = constrain(240.0 / (MaxTemp - d) * val - (d * 240.0) / (MaxTemp - d), 0, 240); } // use the displays color mapping function to get 5-6-5 color palet (R=5 bits, G=6 bits, B-5 bits) return Display.color565(red, green, blue); } // function to get the cutoff points in the temp vs RGB graph void Getabcd() { a = MinTemp + (MaxTemp - MinTemp) * 0.2121; b = MinTemp + (MaxTemp - MinTemp) * 0.3182; c = MinTemp + (MaxTemp - MinTemp) * 0.4242; d = MinTemp + (MaxTemp - MinTemp) * 0.8182; } // function to draw a legend void DrawLegend() { //color legend with max and min text j = 0; float inc = (MaxTemp - MinTemp ) / 160.0; for (ii = MinTemp; ii < MaxTemp; ii += inc) { tft.drawFastHLine(260, 200 - j++, 30, GetColor(ii)); } tft.setTextSize(2); tft.setCursor(245, 20); tft.setTextColor(TFT_WHITE, TFT_BLACK); sprintf(buf, "%2d/%2d", MaxTemp, (int) (MaxTemp * 1.8) + 32); tft.print(buf); tft.setTextSize(2); tft.setCursor(245, 210); tft.setTextColor(TFT_WHITE, TFT_BLACK); sprintf(buf, "%2d/%2d", MinTemp, (int) (MinTemp * 1.8) + 32); tft.print(buf); } // END OF CODE

About Author

Calendar

2020 年 4 月
 12345
6789101112
13141516171819
20212223242526
27282930