Prettify Raspberry Pi shell with oh my zsh

Although the Raspbian OS provides users with a nice GUI, I still prefer using shell to complete most of my tasks. However, the built in terminal, based on bash, is a little bit boring and ugly. So I decide to use oh-my-zsh to make it look cool and fun.

Firstly, you have to install zsh to replace bash.

sudo apt-get install zsh

Then set zsh as default shell

chsh -s /bin/zsh 

But by now, the shell terminal still looks not cool. Let’s use oh-my-zsh to prettify it. Firstly, install it from GitHub through wget

sh -c "$(wget https://raw.githubusercontent.com/robbyrussell/oh-my-zsh/master/tools/install.sh -O -)"

Now restart the terminal you’ll see something different, something much cooler than the original bash shell. You can also switch to other themes according to the official zsh instructions here.

As for me, I’m using the “Agnoster” theme so I can see Git Status. And this is not enough. Let’s make the zsh shell more developer friendly with auto-suggestion and syntax highlights.

Firstly, install the plugins under zsh plugin folder.

git clone git://github.com/zsh-users/zsh-autosuggestions $ZSH_CUSTOM/plugins/zsh-autosuggestions
git clone https://github.com/zsh-users/zsh-syntax-highlighting.git ${ZSH_CUSTOM:-~/.oh-my-zsh/custom}/plugins/zsh-syntax-highlighting

Then add it into your .zshrc file

vim ~/.zshrc
plugins=(git zsh-autosuggestions autojump zsh-syntax-highlighting)

Now restart the terminal and enjoy coding with shell!

About Author

Calendar

2020 年 3 月
 1
2345678
9101112131415
16171819202122
23242526272829
3031