New Revision of Jetson Nano Dev Kit – Now supports new Jetson Nano Module

You’ve probably heard of the Jetson Nano Developer Kit which is able to run modern AI workloads at unprecedented size, power, and cost.

It is now getting refreshed! The A02 Jetson Nano carrier board for the old Developer kit will be now replaced with a new B01 revised carrier board.

What is different?

Firstly, the B01 developer kit carrier board is now compatible with the new Jetson Nano module for those who are looking to design a product. The Jetson Nano module comes along with collateral necessary too for users to be able to create form-factor and use-case, specific carrier boards.

In addition, the carrier board has also been updated to support the production of an upcoming Jetson Xavier NX Module which would be available in the coming March 2020.

Secondly, there are some minor changes in the peripherals on the carrier board of Jetson Nano Developer Kit B01. Here are some photos highlighting the changes of the Jetson Nano Developer Kit carrier board:

In summary, here are the changes that were done to the new B01 Jetson Nano Developer Kit Carrier Board:

  • 1 additional camera connector (J49)
  • Removed Button header (J40)
  • Removed Serial Port Header (J44)
  • Changed the position of Power Select Header (J48)
  • Change the position of camera connector 1 (J13)

Interested in designing a carrier board for the Jetson Nano? You can download the full design files at Jetson Download Centre.

Lastly, the refreshed B01 developer kit is now updated with Nvidia newly released Jetpack 4.3 which includes new versions of TensorRT, cuDNN, improved AI inference performance by 25% which further improves the performance and efficiency of DLA, CSI and encode with containers. In addition, Jetpack 4.3 also includes a new Debian package based installation mechanism for all JetPack components.

To find out more about Jetpack 4.3 new features, you can check out our other blog!

What does it cost?

For the new Jetson Nano Development Kit B01, you can get it at the same price as the previous A02 model at only $99!

Where can I get the new NVIDIA Jetson Nano Development Kit-B01?

Well, you can get it right here at Seeed! We currently have the NVIDIA Jetson Nano Development Kit-B01 up for pre-orders now at only $99! Get yours now and get started on your Machine Learning and AI journey now!

Questions?

Do you have any questions regarding the new Jetson Nano Developer Kit B01? You can comment down in the comments section down below or post any questions to the NVIDIA Jetson Nano Forum.

About Author

Calendar

January 2020
M T W T F S S
 12345
6789101112
13141516171819
20212223242526
2728293031