SenseCAP LoRaWAN Contributes to Smart Greenhouse, Monitoring Environmental Data for Growing Tropical Fruits in Shandong, Northern China.

Poverty alleviation has been one of the top priorities in China’s modern social development. In order to help farmers increase income and improve living conditions, the Chinese government encourages farmers to grow fruits or crops that have higher economic yields.

While fruits that have always been grown in the southern regions, such as lemon, wax apple, dragon fruit, and papaya, have earned increasing popularity in the north, their prices are also relatively higher in the northern markets. Thus farmers in the north can earn higher income if they grow the southern produce rather than the usual northern fruits or crops.

In this case, farmers in Laiwu in Shandong Province embrace the initiative of “growing southern fruits in the north,” in the National Smart Agriculture Industrial Park located in the county.

(Greenhouses in the Smart Agriculture Industrial Park in Laiwu, Shandong Province)

While the farmers were experimenting growing wax apples in one greenhouse at the Industrial Park, they came across some obstacles:

  • The greenhouse environment needs to be strictly monitored and controlled to simulate the environment in the south, or the fruit quality would be compromised.
  • The management cost is high. A system to automatically control the fertilizer, ventilation, thermal and irrigation system is in need.

Seeed was more than happy to take part in this project at the invitation from our partner, a Beijing-based system integrator for agriculture. By deploying SenseCAP in the greenhouse, the following environmental data was collected and monitored in real-time:

  • CO2
  • Light intensity
  • Soil temperature
  • Soil moisture
  • Soil electrical conductivity
  • Photosynthetically active radiation

The data was collected via LR Sensor Nodes and sent to the cloud via the LR Gateway.

While Seeed SenseCAP provides the wireless sensor network solution to collect and monitor environmental data, our partner integrates SenseCAP solution with the controlling system to achieve the following goals:

  • Automatically fertilize and irrigate the plants: When SenseCAP detects deficiency (lower than the preset value) in soil moisture or fertilizer, it triggers the fertilizing and irrigation systems to fertilize and water.
  • Automatically turn on the ventilation system: SenseCAP is connected to the ventilation system, which is activated to cool the greenhouse when the temperature is detected to be higher than the preset value for desired growth.
  • Automatically manage the thermal blanket: The greenhouse thermal blanket helps to retain 95% of the radiant heat and minimizes condensation by containing air, moisture, and vapor in the greenhouse. When SenseCAP is connected to the control system of the thermal blanket, the system can be triggered to fold or unfold the blanket based on the environmental data.

The agriculture sensors and gateways deployed in the greenhouse include the followings:

This is the pilot run of IoT application in “southern fruits grown in the north” scenario, and we are happy that Seeed SenseCAP plays a role in contributing to this initiative. It could gradually collect and accumulate important data for farming experts to provide evaluation for smart agriculture and precision farming, which will eventually further benefit farmers.

“Working with Seeed has been a great pleasure. It’s really useful to introduce SenseCAP, the industrial sensor network solution to our smart agriculture park, as it shows us precise data and helps our existing system to perform automatically. This creates a much better growing environment for the wax apples. We have had a lot of support from the Seeed technical team”

comments Han, Greenhouse Project Expert at our partnered System Integrator

With SenseCAP deployed in the greenhouse in April of 2019, we received a package of freshly-harvested wax apples from the farmers in August. The wax apples actually tasted sweeter than those grown in the south, thanks to the longer daylength (higher light intensity) in the north during summertime.

This project also helps contribute to the following Sustainable Development Goals.

Partners:

  • Laiwu National Smart Agriculture Industrial Park

What is SenseCAP?

SenseCAP is a series of industrial IoT products. Its LoRaWAN version is based on LoRaWAN protocol and deployable worldwide with multiple ISM bands. SenseCAP is encapsulated in an IP66 enclosure, making it applicable in outdoor remote sensing scenarios such as Smart Farming, Smart City, and other IoT applications that need low-power, long-distance, and long-term data collection.

Here’s the newest video of the SenseCAP S210x Series unboxing and shows how to deploy in your area

Updates May 2020: SenseCAP LoRaWAN sensors and gateways are currently available for purchase. If you have any questions, feel free to leave a comment here, email us (iot[at]seeed[dot].cc), or join the discussion at Seeed Forum.

Other User Cases

More Info

About Author

Calendar

2019 年 12 月
 1
2345678
9101112131415
16171819202122
23242526272829
3031