Ubuntu 19.10 official support for Raspberry Pi 4 does not support 4GB version

With the release of Ubunutu 19.10, many Raspberry Pi users are excited as Canonical has announced that it will provide official support for the Raspberry Pi 4.


“With the Raspberry Pi 4 Model B, developers get access to a low-cost board, powerful enough to orchestrate workloads at the edge with MicroK8s.”


During Ubuntu 19.10 announcement, said Canonical

However, currently, the Ubuntu 19.10 only offer official support for the Raspberry Pi 1GB and 2GB versions. This is due to a kernel bug which causes USB ports not being supported out of box in the official arm64 image of the Raspberry Pi 4GB RAM version. Ubuntu have identified the bugs and fixes and are currently testing these fixes extensively, so users do not have to worry as updates will most likely come in a few weeks time.

Here is Ubuntu current plan for Raspberry Pi 4:

Ref: Ubuntu

What can users do?

Currently, Ubuntu released a temporary solution for users who have a Raspberry Pi 4 GB which enable the USB to work. Users will have to edit the file /boot/firmware/usercfg.txt to limit the RAM to 3GB instead of 4GB by keying this following code:

total_mem=3072

For more information and updates about the situation, you can check out Ubuntu blog and forum.

You can also check out our blog on the release notes of Ubuntu 19.10 for Raspberry Pi 4 here.

Haven’t gotten a Raspberry Pi 4 for yourself yet? What are you waiting for? Get a Raspberry Pi 4 Computer Model B 2GB which has Ubuntu 19.10 official support or a Raspberry Pi 4 Computer Model B 4GB here now at Seeed!

About Author

Calendar

2019 年 11 月
 123
45678910
11121314151617
18192021222324
252627282930