Build Your Own Raspberry Pi 4 Retro Game Console – Retropie

Turning your Raspberry Pi into a Retro Game Console has always been a popular and fun project. With the release of the Raspberry Pi 4, with faster processing speeds and better performance, it has the potential now to run games that were previously beyond Pi’s power!

There are various gaming Emulators out there right now for the Raspberry Pi like Retropie, Recalbox, Lakka and many more. Today, we are going to look at one of our favourite gaming Emulators: Retropie. Through this blog, you will learn:

  • What is RetroPie?
  • What do you need to run RetroPie?
  • How to Install RetroPie on your Raspberry Pi 4
  • Tips on Improving your Retro Game System

SALE on Raspberry Pi 4 Accessories!

Before you move on, we have good news for you makers! Right now, Seeed is having a sale on Raspberry Pi 4 accessories!

Don’t miss out! Use code: ACCESSORIES10 to get 10% off selected Raspberry Pi 4 accessories! Click here to check out what’s on sale!

And now, without further ado, let’s dive right into RetroPie!


What is RetroPie?

RetroPie builds upon Raspbian, EmulationStation, RetroArch and other projects which allow you to turn your Raspberry Pi not only into a retro-gaming station but also as an awesome one-stop entertainment system.

The Retropie not only act as an EmulationStation where you can launch and play your games, it also features KODI which is a personal media centre that means you now, not only have games, but you have access to movies, songs and many more!

In addition, the RetroPie has a variety of user-created themes for EmulationStation and also supports over 50 Retro gaming systems for the Raspberry Pi like the Atari Lynx, Dreamcast, Game Boy Advance, GameCube, MAME, Nintendo 64 (N64), PlayStation 2 and 43 more!


What do you need to get started?

We recommend the Raspberry Pi 4 due to its processing speeds and performance. You can still use the older versions of the Raspberry Pi, but it may not have full game compatibly and speed.

Raspberry Pi 4B – Starter Kit – 4GB($79.80)

This starter kit has all the basic essentials, including:

  • Raspberry Pi 4 Computer Model B 4GB
  • Wall Adapter Power Supply – 5VDC 3A Type-C
  • Micro SD Card with Card Reader-32GB(Class 10) 
  • ABS H-Type Black Case for Raspberry Pi 4 B (It Contains Fans and Heat Sinks)
  • Micro HDMI to Standard HDMI Male Cable – 1m(Support Pi 4)
  • Cat6 Ethernet Cable – 1 Meter

Already have some of these parts and only require some of these accessories? You can get them individually here on our Bazaar!

Raspberry Pi Acrylic DIY Retro Game Arcade Kit ($129.00)

This acrylic DIY Retro Game Arcade Kit is simple to set up as you just have to download the Game ROMs from the internet and upload it to your Raspberry Pi and restart and your controller is good to go!

Experience retro arcade gamic as it was meant to, with the original joystick and buttons layout!

We also offer a retro game kit for double players here($69.99) and Single players here.($36.99)

15.6 Inch 1920×1080 Full HD IPS Touch Screen Portable Monitor($169.00)

Take note that any TV or monitor will work fine too! However, if you do not have a monitor or looking for a new one, our Touch Screen Portable Monitor will be a perfect choice for you!

It is high quality but cost-effective multifunction monitor which features an excellent visual experience, supports 1080P FHD @85Hz, and has a wide viewing range of 178 degrees, 400cd/m2 brightness LED backlight, 1000:1 contrast ratio. It is also ultra-thin and ultra-light! With a thickness of 12mm and weight of 720g, which makes this monitor portable too!

Apart from your Raspberry Pi 4, the display supports notebooks, mobile phones, BeagleBone and other SBC, PS4/Xbox/Nintendo Switch and other game consoles thanks to its multiple video input interfaces.


How to Install RetroPie on Raspberry Pi 4

For this setup, you will have to install RetroPie manually as of this date as RetroPie does not officially support the Raspberry Pi 4 yet. You can follow the guide below to install RetroPie manually.

Step 1: Get Raspberry Pi OS Up and Running

First, download a Raspberry Pi OS Desktop Image using the Raspberry Pi Imager.

To make things easier, preconfigure your WiFi in the RPi Imager using these steps.

Flash the OS image to your SD card using the RPi imager.

Once done, transfer SD card from desktop to your Raspberry Pi 4, and let it boot.

If you need help with completing this step, there are detailed official instructions that you can reference here.

Note: On your first boot, you may wish to update your system with the following commands first:

sudo apt update
sudo apt upgrade

Step 2: Retrieve the RetroPie Files

First, launch a terminal window on the Raspberry Pi 4 on the top left-hand corner of your screen.

Next, download RetroPie setup files by keying in:

sudo apt install git lsb-release
cd
git clone --depth=1 https://github.com/RetroPie/RetroPie-Setup.git

Step 3: Run the Setup

cd RetroPie-Setup
chmod +x retropie_setup.sh
sudo ./retropie_setup.sh

Step 4: Install RetroPie

Source: RetroPie

In the GUI that pops up, select Basic Install >> Quick Install. This will install the core and main packages of RetroPie.

Step 5: Copy ROMs to ROMs Directory

Copy your ROMs (Game Files) into the ROMs directory, which can be found at:

~/RetroPie/roms

Make sure you place the ROMs in the correct subdirectory which corresponds to the device you are emulating.

Step 6: Open EmulationSystem

After installation, begin your emulation session by running the following in a terminal window.

emulationstation

Voila! It should bring you to this screen where you can then configure your controllers and start playing your games!

Source: MakeUseof

Improving Your Retro Gaming System

Now you got your own awesome Retro Gaming system, but feel that it is not fast or good enough? Well are some tips that you can make your retro gaming experience even better! Not only does it work for the RetroPie, it will work for other gaming emulators like Recalbox, Batocera, Pi Entertainment system, Lakka and PiPlay (previously PiMAME) too!

Use a Reliable Power Supply

Using your mobile phone charger is probably not the best way to power your Raspberry Pi 4 when you are using an emulator that requires a tad bit more power.

With a poor power supply, your Raspberry Pi performance without a doubt will be affected which means slower games.

How can we solve this problem? Well, use a reliable official Raspberry Pi power supply which you can get here at Seeed!

Raspberry Pi Official Power Supply 15.3W USB-C with 1.5M Cable – UK Plug 5.1V 3A White

Cannot use a UK plug? We also offer various different plugs like the EU plug and US Plug here! We also offer a black version with the US plug here!

Use a Controller

You can’t possibly play N64 or MAME arcade games with a keyboard, right? By using an authentic controller, it can elevate your gaming experience and truly bring you back to the past.

Our Raspberry Pi Acrylic DIY Retro Game Arcade Kit will bring you back in time and allow you to relive your past joys!

This arcade kit is 1. Easy to Setup, 2. High Performance, 3. Highly Integrated, and has a 4. Sleek Appearance!

Here is a video of the easy setup and the entire kit in action!

Source: kevin Deng

Overclock your Raspberry Pi

If you want better and faster performance, overclocking your Raspberry Pi will be the way to go to boost your frame rates while gaming. It brings your Raspberry Pi 4 from a base clock of 1.5GHz, all the way up to 2.147GHz! That’s a lot of power!

Overclocking is easy, and you can follow our comprehensive guide on how to do so here. Do take note that you will need a cooler as an overclocked Pi will tend to run hot – resulting in potential damage!

Blink Blink ICE Tower CPU Cooling Fan for Raspberry Pi

It has a tower structure with a 5 mm copper tube, multi-layer heat sinks, 7 powerful fan blades.

In the case of overclocking, it can reduce the temperature of the Raspberry Pi from 80℃ to 40℃. With the help of this super fan, you can now unlock the powerful performance of the Raspberry Pi 4.

Pick one up on the Seeed Online Store by clicking here!


Summary

That is all for how on how to build your own Raspberry Pi 4 RetroPie game console! With tips on how to improve the performance of your Raspberry Pi 4, you can now enjoy your retro games smoothly just like back in the days!

You can also use your Raspberry Pi 4 in many other ways apart from a retro gaming console! Interested? Check out our blog on the Top 40 Raspberry Pi 4 Projects That You Must Try Now to find out more!

About Author

Calendar

October 2019
M T W T F S S
 123456
78910111213
14151617181920
21222324252627
28293031