Instruction on how to use NVIDIA Jetson Nano with Grove
If you want to run Grove sensors on Jetson Nano, the best way is to use the Grove.py python Library provided by Seeed Studio.
There are more than 20 Groves supporting Jetson Nano now and we are keeping updating more.
See the current sensors supporting Jetson Nano and how to use them:
https://github.com/Seeed-Studio/grove.py/blob/master/doc/README.md
For details about how to install the Grove.py library:
https://github.com/Seeed-Studio/grove.py/blob/master/README.md#installation
Grove Installation Guide
(If you are familiar with the Linux operation system, you can skip this guide and directly refer to the link provided above.)
You only need to perform below steps in a brand new Jetson Nano official Image (click here for Jetson Nano Quick Start Guide), make sure your network works well.
sudo apt-get update
sudo apt-get install curl
Now you can start the installation of grove.py
Step1:
curl -sL https://github.com/Seeed-Studio/grove.py/raw/master/install.sh | sudo bash -s –
Please pay attention to check the final execution result when installing. If FAILED is displayed and you are unable to solve the failure by yourself, please submit new issue in the current repository. Please describe the issue in detail.
Step2:
git clone https://github.com/Seeed-Studio/grove.py
cd grove.py
# Python2
sudo pip install .
# Python3
sudo pip3 install .
Run Grove on Jetson Nano:
After a successful installation, you can use the Grove modules based on the support list of Jetson Nano.
1. First, you need a Grove Base Hat for Raspberry Pi :
The pin header of Jetson Nano is compatible with Pi, however, the function is not completely compatible. Please refer to the table provided by Seeed Studio for the compatibility of specific functions.
The Grove Base Hat is connected like this:
![](https://blog.seeedstudio.com/wp-content/uploads/2019/04/屏幕快照-2019-04-19-上午10.19.27-1030x633.png)
Please pay attention to the pin alignment, do not insert to the wrong position, otherwise it may cause damage to the Grove Base Hat, even the damage of the Jetson Nano Board.
2. Plug in the Grove module.
If it is an I2c module, you can execute it on the Jetson Nano terminal:
sudo i2cdetect -r -y 1
Check if the corresponding I2c address can be scanned. If the scanning failed, please pay attention to the wiring.
3. Execute the corresponding python script command.
Noted that the execution of the python script requires root privileges. For example, when driving an OLED Display 1.12 inch (V1.0) module, you need to do this:
cd grove.py
sudo python grove/display/sh1107g.py
The Grove.py directory is the git repository that was previously downloaded at install time. Usually Oled will display some program-predefined content.
Demo and Software support
We made a demo kit and provided software support for the demo kit.
![](https://blog.seeedstudio.com/wp-content/uploads/2019/04/屏幕快照-2019-04-19-上午10.55.44.png)
The Groves included in the kit:
- OLED Display 1.12 inch – v1.0
- 12 key capacitive i2c touch sensor(MPR121)
- 3-Axis digital accelerometer (ADXL372)
- UV sensor VEML6070
- Thumb joystick v1.1
You can download software here:
https://github.com/linux-downey/jetson_nano_demo_kit_example